This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

RTOS: AM57XX eMMC/SD data transfer by ADMA does not work on RTOS.

Tool/software: TI-RTOS

I have looked at the below RTOS SDK
  pdk_am57xx_1_0_9
and Doc
  spruhz7h.pdf
    AM571x(SR2.0,SR1.0) AM570x(SR2.1,SR2.0)
    SitaraTM Processors
    Technical Reference Manual
    Literature Number: SPRUHZ7H
    August 2015?Revised May 2018
      Chapter 25 eMMC/SD/SDIO
        25.4.5 DMA Modes
        25.4.5.1 Master DMA Operations

Because I use ADMA, but ADMA is not working.
Interrupt Status Register MMCHS_STAT[0] CC BIT is completed, but MMCHS_STAT[1] TC BIT is No transfer complete.

Do you have any missing considerations in running ADMA?
It is implemented by the method shown in 25.4.5.1 Master DMA Operations and  25.5.1.2.1.3 Read/Write Transfer Flow in DMA Mode With Polling.

It is necessary to set for registers not described as ADMA, DMA in the technical manual?
Consider interrupts? etc..

Is there anything necessary to running it?

Customized source code excerpt:
-------------------------------------------
typedef struct {
uint16_t attribute;
uint16_t length;
uint32_t address;
} sdhUsdhcAdmaBd_t;
//ADMA Descriptor Table
sdhUsdhcAdmaBd_t adma_descriptor_table[100];

.
.
.

static MMCSD_Error MMCSD_v1_transfer(MMCSD_Handle handle,
MMCSD_v1_Transaction *transaction)

.
.
.
MMCSD_osalCache_wbInv(object->dataBufIdx,(transaction->blockSize * transaction->blockCount));
for(i=0;i<(transaction->blockCount/127) + ((transaction->blockCount%127 != 0) ? 1:0);i++){
adma_descriptor_table[i].address =(uint32_t)MMCSD_soc_l2_global_addr((uint32_t)&object->dataBufIdx[i*0xFE00]);
adma_descriptor_table[i].length = (uint16_t)(0xFE00);
adma_descriptor_table[i].attribute = (uint8_t) (0x20 | 0x01);
}
adma_descriptor_table[i-1].attribute |= 0x02;
if(transaction->blockCount%127 != 0){
adma_descriptor_table[i-1].length = (uint16_t)(transaction->blockCount%127)*512;
}
MMCSD_osalCache_wbInv(adma_descriptor_table,sizeof(adma_descriptor_table));

/* Set MMCHS ADMASAL register.*/
MMCSDAdmaSetADMASAL(hwAttrs->baseAddr,(uint32_t)MMCSD_soc_l2_global_addr((uint32_t)adma_descriptor_table));

/* Others Register setting used for ADMA */
MMCSDAdmaSetRegister(hwAttrs->baseAddr);
.
.
.
HSMMCSDCommandSend(hwAttrs->baseAddr, &cmdObj);
.
.
.
void MMCSDAdmaSetADMASAL(uint32_t mmcsdBase, const uint32_t address)
{
HW_WR_REG32((mmcsdBase + CSL_MMCHS_ADMASAL), address);
}

void MMCSDAdmaSetRegister(uint32_t mmcsdBase )
{
uint32_t regVal = 0U;

HSMMCSDIntrStatusEnable(mmcsdBase, HS_MMCSD_INTR_MASK_ADMAERROR);
HSMMCSDIntrStatusEnable(mmcsdBase, HS_MMCSD_INTR_MASK_DMA);

regVal = HW_RD_REG32(mmcsdBase + CSL_MMCHS_CON);
regVal |= CSL_MMCHS_CON_DMA_MNS_MASK;
HW_WR_REG32((mmcsdBase + CSL_MMCHS_CON), regVal);

regVal = HW_RD_REG32(mmcsdBase + CSL_MMCHS_HCTL);
regVal |= 0x10;
HW_WR_REG32((mmcsdBase + CSL_MMCHS_HCTL), regVal);
}

-----------------------------------