This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Capturing images on dm365 throw J10 imager interface from AD9923A front end

hi all!

I develope tmx320dm365 based system, which must capture images from ICX445AQA throw AD9923A front end. AD9923A front end will be connected throw J10 imager connector on the dm365 board. I succesfully capture images from composite interface by vpfe /dev/video0.

I have the following questions:

1) Can i use vpfe /dev/video0 intrface to grab images throw J10 conenctor? If so, which driver i will use (mt9t001 or other one)? Discussion http://e2e.ti.com/support/dsp/davinci_digital_media_processors/f/100/t/7646.aspx does not clear situation. Writing driver for this common situation seems to be strange.

2) Discussion http://e2e.ti.com/support/embedded/f/354/p/61601/220861.aspx get me to capture_prev_rsz_onthe_fly_bayer, which require  input subdev with "RAW" name. I see no such subdevs in the git kernel (i use 2.6.32). I see "RAW" mt9t001 device in MVL 2.6.18 kernel. Is there mt9t001 or other "RAW" device support in the git 2.6.32 kernel?

Thanks, Alexandr Dmitriev

Novgorod State University