Tool/software: Linux
Hello Sir, With reference to AM3359 Sitara processor, 1.Our customer requires to RESET the Processor by applying External Reset signal.In which pin of processor we should connect this External Reset signal? 2.Currently in our board we are receiving this External Reset signal in a GPIO pin of processor and when this pin goes low we are calling reboot command of the processor, is this correct or we have to do something else? Kindly help us in this issue at the earliest. Thanks & Regards vamsi