Hi, I'm trying to flash (Texas Instruments Windows CE NAND) X-Loader on BeagleBoard using EVMFlash app.
I'm using UART connection, holding USER button while releasing RESET button.
This error message is being issued:
Download [00:29:05]: [00] Opening UART/USB connection
Download [00:29:05]: [00] Waiting for target to reset
Download [00:29:07]: [00] Unable to read ASIC ID. Searched 32 bytes of data and did not find start of ASIC ID
Download [00:29:07]: [00] Releasing UART/USB connection...
Download [00:29:07]: [00] Error occurred during ROM-code connect phase, return code 0xFFFFFFFE
Download [00:29:07]: [00] Dl connect operation failed. Error code: 0xFFFFFFFE
The same message appears both on XP and win 7 machines.
Has anyone faced similar issue or have some pointers how to solve this?
Thanks,
Teo