Part Number: TDA3
Hi,
When we enable one pass WDR mode with OV10640 with AEWB algorithm, we are observing pink tint at the saturation regions.
We observed that the pink tint is the result of Red and Blue white balance gains applied to the IPIPE. So we applied white balance Red and Blue gains on the sensor instead of IPIPE.
While the tint has reduced, artifacts are still visible at the saturation regions. What could be the reason for this color artifact at the saturation region?
Is this the problem with sensor's WDR combine / tone map module or the GLBCE tonemapping in the IPIPEIF? Could this issue can be fixed by changing either sensor or GLBCE parameters?
P.S: We are observing the issue in two pass WDR also.
Regards,
Navinprashath.R.R