Part Number: AM4376
Tool/software: Linux
Hi Sir
Based on the latest version I2C-BUS spec. Tf need to be more than 20*(Vdd/5.5V) when clk freq is more than 100kHz(e.g. Fast-mode). But I2C fall time of AM4376 is very short, about 1ns.
When AM4376 I2C BUS connects with other I2C-bus slave devices, is it necessary to make the fall time of I2C-bus meets the requirements of the slave devices. And if yes, how to achieve it ?
BR
Yimin