When I run the Graphic LCD Test of the BSL, instead of being stable, the color strips would move and the screen would keep flashing, Is there something wrong with it? if yes, what goes wrong?
Besides that, when running the RAM Test of the BSL, the block of memory should first be written with 0x55555555 and verify, then 0xAAAAAAAA and verify again, but then the test fails everytime. There are always some blocks of memory not written into the expected data. Is there something wrong with the RAM?
sorry if I am not explaining clearly,
and thanks everyone who help.