Hi ,all kind and handsome men,
I want to let my RTC works normally in DM365.
But when the system reboots,the RTC is reset and I can't save the time I set last time.
The startup log is as follows:
Time: timer0_1 clocksource has been installed.
Clock event device timer0_0 configured with caps set: 08
Switched to high resolution mode on CPU 0
rtc_davinci_dm365 rtc_davinci_dm365.0: setting the system clock to 2000-01-01 00:00:00 (946684800)
And I am sure that I compile the RTC into the kernel .
But I don;t know why it always rewrite the time.
My LSP version is psp_02_10_00_14
Thank you.