We're streaming MPEG4 video from a DM365 hosted application. At the receiving end we save it to file.
The saved file will play in several players (mplayer, VLC, etc) but will not play in Quicktime. The top 1/5 or so of the image is good. The second 1/5 is shifted over a bit (as if image width or scan length is incorrect). From there down it gets worse, including degraded chroma information.
We've check all config parameters and SDP file values and they all look good.
Are there any known issues playing MPEG4 through Quicktime? Any suggestions?
Thanks!