Hi All,
The module number of VPSS DAC in the PSC controller of the DM355 is not clear. sprufb3.pdf says it is 41 and tms320dm355.pdf says it is 40. Which number is correct ? Please clarify.
regards,
Dilip.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi All,
The module number of VPSS DAC in the PSC controller of the DM355 is not clear. sprufb3.pdf says it is 41 and tms320dm355.pdf says it is 40. Which number is correct ? Please clarify.
regards,
Dilip.
40= MJCP
41= VPSS VDAC
Datasheet will be fixed.
Hi Brad Griffis,
Thanks for the information.
But, the problem is if I try to enable the VPSS VDAC module it's not enabled. It always show the status as disabled. Is there any specific sequence of steps to enable the VPSS VDAC ?
regards,
T.Dilip Chakravarthy.
I believe there are additional registers described in the VPBE UG (e.g. selecting clock source, enabling clock for DAC...)