Tool/software: Linux
when i want to fetch source code (executed fetch_source.sh), it failed , show error message like below:
"
fatal: unable to connect to git.omapzoom.org:
git.omapzoom.org[0: 198.47.28.210]: errno=Connection refused
"
even i try fetch source code via a VPN, it is the same error.
and i nmap the git.omapzoom.org:
"
Starting Nmap 6.40 ( http://nmap.org ) at 2018-12-30 18:03 PST
Nmap scan report for git.omapzoom.org (198.47.28.210)
Host is up (0.28s latency).
PORT STATE SERVICE
80/tcp open http
8008/tcp filtered http
9418/tcp filtered git
"
and i try fetch source manually
"git clone http://git.omapzoom.org/kernel/omap.git"
"git clone git://git.omapzoom.org/kernel/omap.git"
but always failed...
"
$ git clone git://git.omapzoom.org/kernel/omap.git
Cloning into 'omap'...
fatal: unable to connect to git.omapzoom.org:
git.omapzoom.org[0: 198.47.28.210]: errno=Invalid argument
"
"
$ git clone git.omapzoom.org/.../omap.git
Cloning into 'omap'...
error: Unable to get pack index git.omapzoom.org/.../pack-490026bd27b456719a336d932f6a7f6779c9a8d2.idx
error: Unable to find f5f1aabd7b9a6c8c13ab6115c49b42c6b1ae30e7 under git.omapzoom.org/.../omap.git
Cannot obtain needed object f5f1aabd7b9a6c8c13ab6115c49b42c6b1ae30e7
error: fetch failed.
"
please help me how to solve this ?