Other Parts Discussed in Thread: PRU-ICSS-INDUSTRIAL-SW
Hi,
!! Thanks in advance !!
I want to use the ether phy 88E1512(MARVELL CHIP) for the PTP protocol on AM5728 processor.
My queries are
1)Is the AM5728 support PTP protocol?If yes,how the protocol is implemented and what all the hardware connection
required for the same.Is there any driver need to be implemented for the same?
2)I want to connect the other RGMII port of the AM5728 to the Artix FPGA via RGMII MAC-TO-MAC connection.Is the MAC-TO-MAC
solution is feasible ?what are all the pin connection required for the same?
share the document for the same if available.
Thanks
ASHOK KUMAR SIHAG
7975708272