This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

RTOS/TDA2PXEVM: Issue while using networkRx with .YUV (YUV420P) video as input

Part Number: TDA2PXEVM


Tool/software: TI-RTOS

Hi,

I'm using TDA2PX EVM and visionSDK 3.05.

I'm using usecase NetworkRx  -> display. I'm giving input.yuv as input which has following specifications:

codec : Planer 4:2:0 YUV (I420)

Resolution : 640X480

FPS: 30

There is no assertion or error but output is not same as that of input (seen from VLC media player). I have attached output of usecase and screenshot of VLC player for reference

    

How should I proceed with this?

Is there issue of 420p to 420sp compatibility as in networkRx  set params the format set is YUV420SP? If yes, please suggest changes needed to be done for yuv420p ? or is there is way to convert yuv420p to yuv420sp ?