This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Compiler/TDA3: TDA3x

Part Number: TDA3

Tool/software: TI C/C++ Compiler

How can I run the usecase of null_src_display on the EVM of TDA3x. I have set the UC_null_src_display=yes  of uc_cfg.make,other UC_xxxx_xx=no. And the core I open is:

PROC_IPU1_0_INCLUDE=yes PROC_IPU1_1_INCLUDE=no   PROC_DSP1_INCLUDE=yes      PROC_DSP2_INCLUDE=no       PROC_EVE1_INCLUDE=no

The chose information of the serial port is as below:   I cannot choose any of them

Vision SDK Usecases,
[IPU1-0] --------------------
[IPU1-0] 1: Single Camera Usecases
[IPU1-0] 2: Multi-Camera LVDS Usecases
[IPU1-0] 3: AVB RX Usecases, (TDA2x & TDA2Ex ONLY)
[IPU1-0] 4: Dual Display Usecases, (TDA2x EVM ONLY)
[IPU1-0] 5: ISS Usecases, (TDA3x ONLY)
[IPU1-0] 6: TDA2x Stereo Usecases
[IPU1-0] a: Miscellaneous test's
[IPU1-0] c: OPENVX Usecases
[IPU1-0] f: TIDL Usecase