Tool/software: Linux
My board is AM335x Starter Kit
SDK Version:ti-processor-sdk-linux-rt-am335x-evm-05.01.00.11-Linux-x86-Install
Hi,
My AM335x Starter Kit is booted from an SD card. There are a lot of buttons on this board. One of them is the WarmRST button. Today I pressed this button (perhaps some other button, I am not sure), then the board is not reacted. Even if the board is powered back on, nothing happens, and the serial port has no output.
What could be the cause of this problem? Will it change the boot order mode in a certain process? Still some other reasons?
Thank You,
Hefa