Part Number: AM5728
Tool/software: Linux
which DTS file need to be changed in device tree to enable PWM 1, 2 & 3 on TI 57xx-EVM using SDK_5.0.0.15 for TI 5728
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Pavel,
I understand that to enable i need to put below mention statement in linux-kernel/arch/arm/boot/dts/ti/am57xx-evm-common.dtso
&epwmssx {
status = "okay";
};
&ehrpwmx {
status = "okay";
};
where x - 1,2,3
But my main doubt are:
1. Which DTS file need to used to make dtb that can load into target rootfs, As am not able to locate AM57xx-evm.dts file under my compile linux directory mention below, although it has AM57xx-evm.dtb file
/ti-processor-sdk-linux-am57xx-evm-05.00.00.15/board-support/linux-4.14.40/arch/arm/boot/dts
2. And i also seen there is no such compatibility mention in pwm-tipwmss.c and pwm-tiehrpwm.c for TIAM57xx-EVM in drivers. So how these pwm drivers can be utilize in that case.
Akash,
akash garg said:1. Which DTS file need to used to make dtb that can load into target rootfs, As am not able to locate AM57xx-evm.dts file under my compile linux directory mention below, although it has AM57xx-evm.dtb file
/ti-processor-sdk-linux-am57xx-evm-05.00.00.15/board-support/linux-4.14.40/arch/arm/boot/dts
You need to use am57xx-evm.dtso or am57xx-evm-reva3.dtso depending on which version of the EVM you have. See also below user guide:

akash garg said:2. And i also seen there is no such compatibility mention in pwm-tipwmss.c and pwm-tiehrpwm.c for TIAM57xx-EVM in drivers. So how these pwm drivers can be utilize in that case.
AM57x use "ti,dra746-pwmss", "ti,dra746-ehrpwm" and "ti,dra746-ecap". See below file:
linux-kernel/arch/arm/boot/dts/dra7.dtsi
Regards,
Pavel
Hi Pavel,
Am using AM57xx-Evm revA3 and processor SDK linux 5.0.0.15. As you suggest i update my am57xx-evm-revA3.dts to enable other PWMSS.
Previously /sys/class/pwm shows only pwmchip0 that will be used for LCD backlight. After i enable other PWMSS, am able to access pwmchip2 also.
Also able to configure pwm0 & pwm1 for that and there properties like period, duty_cycle.
But not able to debug there output on ehrpwm3A & ehrpwm3B respective pins.
I configured pin35 and pin37 of P17 connector on EVM as ehrpwm3A & ehrpwm3B respectively using mux_data.h under uboot.
My main requirement to enable two PWM channel of 100KHz of oppositve polarity.