This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TDA3: LDC: affine transform.

Part Number: TDA3

SIMCOP/LDC

input frame 1920x1088

output frame 800x1280

Meshtable: 120x68

Case 1:

I have working code for input frame 1920x1088 to output frame 1280x800 with the use of Simcop. In simcop configuration, we are not using affine transform for this undistortion image. This is working fine.

Case 2:

Now we have to rotate the output image 800x1280 and whereas input image is the same 1920x1088. I am wondering how can I implement this. Do I need to use affine transform feature to rotate the image?

Can you please guide me how can I solve my problem

Best regards,

Naresh