hi ,all
i wonder if dm365 or dm368 's PCLK input IO could recognize a Vpp=800mV and DC=1.34V clock signal correctly ?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
ng,
You will need to apply the datasheet specifications to your system design constraints, in particular the voltage at which you will operate PCLK.
But an input signal that goes from 0.94V to 1.74V will not work. The datasheet will tell you what voltages are required. Look for the VIL and VIH parameters.
Regards,
RandyP
If this answers your question, please click the Verify Answer button below. If not, please reply back with more information.
Hi,
According to the DM365 data sheet, page 72 and page 73, the VIH min is 0.7VDDS_ISIF18_33= 1.197V and VIL max is 0.3VDDS)ISIF18_33=0.513V so it could not recognize the signal you describe here.
Thanks,
Tai