This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

RTOS/TMS320C6657: TMS320C6657 - MT41K512M8 Possible DDR3 Timing Issues

Part Number: TMS320C6657

Tool/software: TI-RTOS

Hello,

I have plugged in values from the Micron MT41K512M8 datasheet into DDR3 Register Calc v4 spreadsheet, but since my part wasn't listed I did the best I could to add the necessary values.

I've been chasing some odd memory behavior in two flavors. One is failed readback values in a simple walking 1's type ram test. The second issue I've noticed is hitting breakpoints for a second time in my main startup thread after it has already executed, and I can't tell if it's a second instance or if somehow the PC has jumped.

With both cases, I figured it would be best to start by asking for a verification of my EMIF configuration registers for a 1066 Data Rate.

DDR_SDTIM1        0x21000018 0CCF36B3
DDR_SDTIM2        0x21000020 308F7FDA
DDR_SDTIM3      0x21000028 557F88AF
DDR_SDCFG        0x21000008 63026B33
DDR_SDRFC (normal)        0x21000010 00001046
DDR_SDRFC
(ext temp)       
0x21000010 00000823
DDR_SDRFC (initialization)        0x21000010 0000411A

Happy new year,

Eric