This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Compiler/TDA2EXEVM: Libc-2.15. so debug library usage problem

Part Number: TDA2EXEVM


Tool/software: TI C/C++ Compiler

The current platform is TDA2EX, and problems were encountered during the use of Valgrind migration, culminating in the confirmation that glibc's library had no debug information.

After checking the solution, copy the cross-compilation tool gcc-linaro-arm-linux-gnueabihf-4.7-2013.03-20130313_linux into the lib directory of the file system libc-2.15.so in the debug directory under libc.

At this point, the system starts up with the following error:

U-Boot 2014.07 (Nov 28 2018 - 11:21:01)

CPU : DRA752-GP ES1.0
Board: DRA7xx
I2C: ready
DRAM: 2 GiB
MMC: OMAP SD/MMC: 0, OMAP SD/MMC: 1
Using default environment

serial# not set, setting...
switch to partitions #0, OK
mmc0 is current device
SD/MMC found on device 0
4853992 bytes read in 247 ms (18.7 MiB/s)
92681 bytes read in 11 ms (8 MiB/s)
Booting from mmc0 ...
Kernel image @ 0x82000000 [ 0x000000 - 0x4a10e8 ]
## Flattened Device Tree blob at 88000000
Booting using the fdt blob at 0x88000000
reserving fdt memory region: addr=85800000 size=10000000
reserving fdt memory region: addr=a0000000 size=6000000
reserving fdt memory region: addr=a6000000 size=fd2000
reserving fdt memory region: addr=b0000000 size=5000000
Loading Device Tree to 857e6000, end 857ffa08 ... OK
Check Max9286 him 0x80

Starting kernel ...

[ 0.000000] GIC CPU mask not found - kernel will fail to boot.
[ 0.000000] GIC CPU mask not found - kernel will fail to boot.
[ 0.929366] Kernel panic - not syncing: Attempted to kill init! exitcode=0x0000000b
[ 0.929366] 
[ 0.938542] drm_kms_helper: panic occurred, switching back to text console
[ 0.945462] ------------[ cut here ]------------
[ 0.950108] WARNING: CPU: 0 PID: 1 at drivers/gpu/drm/omapdrm/omap_crtc.c:617 omap_crtc_apply+0x90/0x9c()
[ 0.959714] Modules linked in:
[ 0.962791] CPU: 0 PID: 1 Comm: init Not tainted 3.14.63 #30
[ 0.968472] Backtrace: 
[ 0.970946] [<c0012128>] (dump_backtrace) from [<c00122c4>] (show_stack+0x18/0x1c)
[ 0.978546] r6:20000193 r5:ffffffff r4:00000000 r3:00000000
[ 0.984267] [<c00122ac>] (show_stack) from [<c06449a0>] (dump_stack+0x80/0xa0)
[ 0.991524] [<c0644920>] (dump_stack) from [<c0046d20>] (warn_slowpath_common+0x70/0x94)
[ 0.999646] r7:00000269 r6:c0395020 r5:00000009 r4:00000000
[ 1.005367] [<c0046cb0>] (warn_slowpath_common) from [<c0046d68>] (warn_slowpath_null+0x24/0x2c)
[ 1.014187] r8:000002d0 r7:00000500 r6:00000000 r5:ecdadd8c r4:ecdae800
[ 1.020960] [<c0046d44>] (warn_slowpath_null) from [<c0395020>] (omap_crtc_apply+0x90/0x9c)
[ 1.029349] [<c0394f90>] (omap_crtc_apply) from [<c03958f4>] (apply+0x24/0x28)
[ 1.036599] r5:00000000 r4:00000000
[ 1.040207] [<c03958d0>] (apply) from [<c0395be8>] (omap_plane_mode_set+0x100/0x148)
[ 1.047986] [<c0395ae8>] (omap_plane_mode_set) from [<c039470c>] (omap_crtc_mode_set+0x11c/0x130)
[ 1.056893] r10:1500000a r9:00000048 r8:eca12594 r7:00000000 r6:00000000 r5:ecdae800
[ 1.064793] r4:05000000
[ 1.067347] [<c03945f0>] (omap_crtc_mode_set) from [<c03731cc>] (drm_crtc_helper_set_mode+0x2a4/0x4bc)
[ 1.076690] r10:ecd88800 r9:ecd889b4 r8:00000001 r7:eca12580 r6:eca12980 r5:ecd889b8
[ 1.084593] r4:ecdae800
[ 1.087147] [<c0372f28>] (drm_crtc_helper_set_mode) from [<c0373c70>] (drm_crtc_helper_set_config+0x764/0x8c0)
[ 1.097187] r10:ecd88994 r9:00000004 r8:ecc68400 r7:ecd889b8 r6:ecd889a0 r5:ecdac5c0
[ 1.105089] r4:ecdae800
[ 1.107643] [<c037350c>] (drm_crtc_helper_set_config) from [<c038550c>] (drm_mode_set_config_internal+0x5c/0xdc)
[ 1.117858] r10:ec8e7b40 r9:ec8e2dc0 r8:00000000 r7:eca16840 r6:ecdac5c0 r5:ecdae800
[ 1.125760] r4:eca166c0
[ 1.128316] [<c03854b0>] (drm_mode_set_config_internal) from [<c03768fc>] (drm_fb_helper_restore_fbdev_mode+0xac/0xcc)
[ 1.139053] r6:ecdac5c0 r5:00000000 r4:00000001 r3:00000000
[ 1.144770] [<c0376850>] (drm_fb_helper_restore_fbdev_mode) from [<c0376958>] (drm_fb_helper_force_kernel_mode+0x3c/0x60)
[ 1.155769] r8:00000000 r7:c09a5794 r6:00000000 r5:c09799c0 r4:eca16840
[ 1.162542] [<c037691c>] (drm_fb_helper_force_kernel_mode) from [<c0376c08>] (drm_fb_helper_panic+0x30/0x3c)
[ 1.172408] r6:00000000 r5:00000000 r4:fffffffe r3:ec8e8000
[ 1.178126] [<c0376bd8>] (drm_fb_helper_panic) from [<c064c45c>] (notifier_call_chain+0x4c/0x8c)
[ 1.186950] [<c064c410>] (notifier_call_chain) from [<c064c4dc>] (__atomic_notifier_call_chain+0x40/0x54)
[ 1.196554] r8:c09a5b94 r7:00000000 r6:c09a5794 r5:ffffffff r4:00000000 r3:ffffffff
[ 1.204372] [<c064c49c>] (__atomic_notifier_call_chain) from [<c064c510>] (atomic_notifier_call_chain+0x20/0x28)
[ 1.214588] r8:ec8e8000 r7:eccc9e40 r6:ec8e7b40 r5:c07d0bc8 r4:c09a5770
[ 1.221358] [<c064c4f0>] (atomic_notifier_call_chain) from [<c064239c>] (panic+0x94/0x1c8)
[ 1.229659] [<c064230c>] (panic) from [<c00490bc>] (do_exit+0x804/0x8cc)
[ 1.236385] r3:ec8e2dc0 r2:00000000 r1:0000000b r0:c07d0bc8
[ 1.242098] r7:eccc9e40
[ 1.244651] [<c00488b8>] (do_exit) from [<c0049298>] (do_group_exit+0x44/0xb8)
[ 1.251901] r7:ecc86fc4
[ 1.254453] [<c0049254>] (do_group_exit) from [<c00542f0>] (get_signal_to_deliver+0x1c8/0x54c)
[ 1.263098] r7:ecc86fc4 r6:ec8e8000 r5:ec8e9ed4 r4:ec8e8000
[ 1.268813] [<c0054128>] (get_signal_to_deliver) from [<c0011698>] (do_signal+0x108/0x408)
[ 1.277109] r10:00000000 r9:ec8e8000 r8:00000000 r7:ec8e9ec0 r6:ec8e8000 r5:ec8e8000
[ 1.285011] r4:ec8e9fb0
[ 1.287564] [<c0011590>] (do_signal) from [<c0011ce0>] (do_work_pending+0x70/0xb0)
[ 1.295163] r10:00000001 r9:ec8e8000 r8:00000000 r7:ec8e9fb0 r6:ec8e8000 r5:ec8e8000
[ 1.303065] r4:ec8e8000
[ 1.305618] [<c0011c70>] (do_work_pending) from [<c000ebc8>] (work_pending+0xc/0x20)
[ 1.313391] r10:b6f56c30 r8:00000000 r7:beb2fa20 r6:ffffffff r5:40000030 r4:b6f45964
[ 1.321292] ---[ end trace d99e58ee3e662755 ]---
[ 1.325936] ------------[ cut here ]------------
[ 1.330576] WARNING: CPU: 0 PID: 1 at drivers/gpu/drm/omapdrm/omap_crtc.c:617 omap_crtc_apply+0x90/0x9c()
[ 1.340179] Modules linked in:
[ 1.343253] CPU: 0 PID: 1 Comm: init Tainted: G W 3.14.63 #30
[ 1.349893] Backtrace: 
[ 1.352361] [<c0012128>] (dump_backtrace) from [<c00122c4>] (show_stack+0x18/0x1c)
[ 1.359960] r6:20000193 r5:ffffffff r4:00000000 r3:00000000
[ 1.365678] [<c00122ac>] (show_stack) from [<c06449a0>] (dump_stack+0x80/0xa0)
[ 1.372934] [<c0644920>] (dump_stack) from [<c0046d20>] (warn_slowpath_common+0x70/0x94)
[ 1.381056] r7:00000269 r6:c0395020 r5:00000009 r4:00000000
[ 1.386774] [<c0046cb0>] (warn_slowpath_common) from [<c0046d68>] (warn_slowpath_null+0x24/0x2c)
[ 1.395593] r8:eca12c80 r7:00000000 r6:ecdae800 r5:ecdaeb84 r4:ecdae800
[ 1.402363] [<c0046d44>] (warn_slowpath_null) from [<c0395020>] (omap_crtc_apply+0x90/0x9c)
[ 1.410753] [<c0394f90>] (omap_crtc_apply) from [<c0395094>] (omap_crtc_dpms+0x68/0x100)
[ 1.418874] r5:ecd88800 r4:ecdae800
[ 1.422481] [<c039502c>] (omap_crtc_dpms) from [<c0395334>] (omap_crtc_commit+0x40/0x6c)
[ 1.430603] r8:00000001 r7:eca12580 r6:eca12980 r5:ecd88800 r4:ecdae800
[ 1.437374] [<c03952f4>] (omap_crtc_commit) from [<c037321c>] (drm_crtc_helper_set_mode+0x2f4/0x4bc)
[ 1.446543] r5:ecd889b8 r4:ecdae800
[ 1.450151] [<c0372f28>] (drm_crtc_helper_set_mode) from [<c0373c70>] (drm_crtc_helper_set_config+0x764/0x8c0)
[ 1.460191] r10:ecd88994 r9:00000004 r8:ecc68400 r7:ecd889b8 r6:ecd889a0 r5:ecdac5c0
[ 1.468092] r4:ecdae800
[ 1.470645] [<c037350c>] (drm_crtc_helper_set_config) from [<c038550c>] (drm_mode_set_config_internal+0x5c/0xdc)
[ 1.480859] r10:ec8e7b40 r9:ec8e2dc0 r8:00000000 r7:eca16840 r6:ecdac5c0 r5:ecdae800
[ 1.488761] r4:eca166c0
[ 1.491313] [<c03854b0>] (drm_mode_set_config_internal) from [<c03768fc>] (drm_fb_helper_restore_fbdev_mode+0xac/0xcc)
[ 1.502051] r6:ecdac5c0 r5:00000000 r4:00000001 r3:00000000
[ 1.507768] [<c0376850>] (drm_fb_helper_restore_fbdev_mode) from [<c0376958>] (drm_fb_helper_force_kernel_mode+0x3c/0x60)
[ 1.518767] r8:00000000 r7:c09a5794 r6:00000000 r5:c09799c0 r4:eca16840
[ 1.525539] [<c037691c>] (drm_fb_helper_force_kernel_mode) from [<c0376c08>] (drm_fb_helper_panic+0x30/0x3c)
[ 1.535405] r6:00000000 r5:00000000 r4:fffffffe r3:ec8e8000
[ 1.541123] [<c0376bd8>] (drm_fb_helper_panic) from [<c064c45c>] (notifier_call_chain+0x4c/0x8c)
[ 1.549947] [<c064c410>] (notifier_call_chain) from [<c064c4dc>] (__atomic_notifier_call_chain+0x40/0x54)
[ 1.559552] r8:c09a5b94 r7:00000000 r6:c09a5794 r5:ffffffff r4:00000000 r3:ffffffff
[ 1.567369] [<c064c49c>] (__atomic_notifier_call_chain) from [<c064c510>] (atomic_notifier_call_chain+0x20/0x28)
[ 1.577585] r8:ec8e8000 r7:eccc9e40 r6:ec8e7b40 r5:c07d0bc8 r4:c09a5770
[ 1.584356] [<c064c4f0>] (atomic_notifier_call_chain) from [<c064239c>] (panic+0x94/0x1c8)
[ 1.592657] [<c064230c>] (panic) from [<c00490bc>] (do_exit+0x804/0x8cc)
[ 1.599383] r3:ec8e2dc0 r2:00000000 r1:0000000b r0:c07d0bc8
[ 1.605093] r7:eccc9e40
[ 1.607645] [<c00488b8>] (do_exit) from [<c0049298>] (do_group_exit+0x44/0xb8)
[ 1.614895] r7:ecc86fc4
[ 1.617446] [<c0049254>] (do_group_exit) from [<c00542f0>] (get_signal_to_deliver+0x1c8/0x54c)
[ 1.626090] r7:ecc86fc4 r6:ec8e8000 r5:ec8e9ed4 r4:ec8e8000
[ 1.631809] [<c0054128>] (get_signal_to_deliver) from [<c0011698>] (do_signal+0x108/0x408)
[ 1.640105] r10:00000000 r9:ec8e8000 r8:00000000 r7:ec8e9ec0 r6:ec8e8000 r5:ec8e8000
[ 1.648005] r4:ec8e9fb0
[ 1.650558] [<c0011590>] (do_signal) from [<c0011ce0>] (do_work_pending+0x70/0xb0)
[ 1.658156] r10:00000001 r9:ec8e8000 r8:00000000 r7:ec8e9fb0 r6:ec8e8000 r5:ec8e8000
[ 1.666056] r4:ec8e8000
[ 1.668608] [<c0011c70>] (do_work_pending) from [<c000ebc8>] (work_pending+0xc/0x20)
[ 1.676381] r10:b6f56c30 r8:00000000 r7:beb2fa20 r6:ffffffff r5:40000030 r4:b6f45964
[ 1.684283] ---[ end trace d99e58ee3e662756 ]---
[ 1.688916] ------------[ cut here ]------------
[ 1.693555] WARNING: CPU: 0 PID: 1 at drivers/gpu/drm/omapdrm/omap_crtc.c:617 omap_crtc_apply+0x90/0x9c()
[ 1.703159] Modules linked in:
[ 1.706232] CPU: 0 PID: 1 Comm: init Tainted: G W 3.14.63 #30
[ 1.712870] Backtrace: 
[ 1.715336] [<c0012128>] (dump_backtrace) from [<c00122c4>] (show_stack+0x18/0x1c)
[ 1.722935] r6:20000193 r5:ffffffff r4:00000000 r3:00000000
[ 1.728654] [<c00122ac>] (show_stack) from [<c06449a0>] (dump_stack+0x80/0xa0)
[ 1.735910] [<c0644920>] (dump_stack) from [<c0046d20>] (warn_slowpath_common+0x70/0x94)
[ 1.744031] r7:00000269 r6:c0395020 r5:00000009 r4:00000000
[ 1.749751] [<c0046cb0>] (warn_slowpath_common) from [<c0046d68>] (warn_slowpath_null+0x24/0x2c)
[ 1.758571] r8:eca12c80 r7:00000000 r6:ecdae800 r5:ecdadd8c r4:ecdae800
[ 1.765342] [<c0046d44>] (warn_slowpath_null) from [<c0395020>] (omap_crtc_apply+0x90/0x9c)
[ 1.773732] [<c0394f90>] (omap_crtc_apply) from [<c03958f4>] (apply+0x24/0x28)
[ 1.780981] r5:ecd88800 r4:ecdae800
[ 1.784588] [<c03958d0>] (apply) from [<c0395d18>] (omap_plane_dpms+0x28/0x34)
[ 1.791845] [<c0395cf0>] (omap_plane_dpms) from [<c03950a0>] (omap_crtc_dpms+0x74/0x100)
[ 1.799971] [<c039502c>] (omap_crtc_dpms) from [<c0395334>] (omap_crtc_commit+0x40/0x6c)
[ 1.808092] r8:00000001 r7:eca12580 r6:eca12980 r5:ecd88800 r4:ecdae800
[ 1.814864] [<c03952f4>] (omap_crtc_commit) from [<c037321c>] (drm_crtc_helper_set_mode+0x2f4/0x4bc)
[ 1.824032] r5:ecd889b8 r4:ecdae800
[ 1.827638] [<c0372f28>] (drm_crtc_helper_set_mode) from [<c0373c70>] (drm_crtc_helper_set_config+0x764/0x8c0)
[ 1.837678] r10:ecd88994 r9:00000004 r8:ecc68400 r7:ecd889b8 r6:ecd889a0 r5:ecdac5c0
[ 1.845579] r4:ecdae800
[ 1.848132] [<c037350c>] (drm_crtc_helper_set_config) from [<c038550c>] (drm_mode_set_config_internal+0x5c/0xdc)
[ 1.858347] r10:ec8e7b40 r9:ec8e2dc0 r8:00000000 r7:eca16840 r6:ecdac5c0 r5:ecdae800
[ 1.866248] r4:eca166c0
[ 1.868800] [<c03854b0>] (drm_mode_set_config_internal) from [<c03768fc>] (drm_fb_helper_restore_fbdev_mode+0xac/0xcc)
[ 1.879538] r6:ecdac5c0 r5:00000000 r4:00000001 r3:00000000
[ 1.885256] [<c0376850>] (drm_fb_helper_restore_fbdev_mode) from [<c0376958>] (drm_fb_helper_force_kernel_mode+0x3c/0x60)
[ 1.896256] r8:00000000 r7:c09a5794 r6:00000000 r5:c09799c0 r4:eca16840
[ 1.903028] [<c037691c>] (drm_fb_helper_force_kernel_mode) from [<c0376c08>] (drm_fb_helper_panic+0x30/0x3c)
[ 1.912893] r6:00000000 r5:00000000 r4:fffffffe r3:ec8e8000
[ 1.918610] [<c0376bd8>] (drm_fb_helper_panic) from [<c064c45c>] (notifier_call_chain+0x4c/0x8c)
[ 1.927433] [<c064c410>] (notifier_call_chain) from [<c064c4dc>] (__atomic_notifier_call_chain+0x40/0x54)
[ 1.937037] r8:c09a5b94 r7:00000000 r6:c09a5794 r5:ffffffff r4:00000000 r3:ffffffff
[ 1.944856] [<c064c49c>] (__atomic_notifier_call_chain) from [<c064c510>] (atomic_notifier_call_chain+0x20/0x28)
[ 1.955071] r8:ec8e8000 r7:eccc9e40 r6:ec8e7b40 r5:c07d0bc8 r4:c09a5770
[ 1.961841] [<c064c4f0>] (atomic_notifier_call_chain) from [<c064239c>] (panic+0x94/0x1c8)
[ 1.970140] [<c064230c>] (panic) from [<c00490bc>] (do_exit+0x804/0x8cc)
[ 1.976867] r3:ec8e2dc0 r2:00000000 r1:0000000b r0:c07d0bc8
[ 1.982579] r7:eccc9e40
[ 1.985130] [<c00488b8>] (do_exit) from [<c0049298>] (do_group_exit+0x44/0xb8)
[ 1.992380] r7:ecc86fc4
[ 1.994931] [<c0049254>] (do_group_exit) from [<c00542f0>] (get_signal_to_deliver+0x1c8/0x54c)
[ 2.003576] r7:ecc86fc4 r6:ec8e8000 r5:ec8e9ed4 r4:ec8e8000
[ 2.009292] [<c0054128>] (get_signal_to_deliver) from [<c0011698>] (do_signal+0x108/0x408)
[ 2.017588] r10:00000000 r9:ec8e8000 r8:00000000 r7:ec8e9ec0 r6:ec8e8000 r5:ec8e8000
[ 2.025489] r4:ec8e9fb0
[ 2.028042] [<c0011590>] (do_signal) from [<c0011ce0>] (do_work_pending+0x70/0xb0)
[ 2.035640] r10:00000001 r9:ec8e8000 r8:00000000 r7:ec8e9fb0 r6:ec8e8000 r5:ec8e8000
[ 2.043541] r4:ec8e8000
[ 2.046095] [<c0011c70>] (do_work_pending) from [<c000ebc8>] (work_pending+0xc/0x20)
[ 2.053868] r10:b6f56c30 r8:00000000 r7:beb2fa20 r6:ffffffff r5:40000030 r4:b6f45964
[ 2.061769] ---[ end trace d99e58ee3e662757 ]---
[ 2.084790] mmc1: BKOPS_EN bit is not set
[ 2.092784] mmc1: new high speed DDR MMC card at address 0001
[ 2.099179] mmcblk1: mmc1:0001 MMC04G 3.57 GiB 
[ 2.103951] mmcblk1boot0: mmc1:0001 MMC04G partition 1 8.00 MiB
[ 2.110128] mmcblk1boot1: mmc1:0001 MMC04G partition 2 8.00 MiB

Above, please also guide, thank you.