Part Number: AM3352
Hi,
I am refering the Figure 6-2/6-3/6-4 in AM335x datasheet(sprs717k.pdf).
I have few questions about RTC_PWRONRSTn specification for AM335x.
1.
I understand as follow:
- RTC_PWRONRSTn should be deasserted after 1 ms elapsed since VDDS_RTC was supplied.
- There is no dependency other powers and signals(1.8V Supplies,VDD_CORE,etc.) for RTC_PWRONRSTn release timing.
Are these correct?
2.
About RTC_PWRONRSTn, how long is the asserted timing required to reset the RTC domain?
As in annotation A, is it required at least 1ms to reset?
Regards,
Yasun