This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

RTOS/66AK2H12: 66AK2H12: [EVMK2H] How Can I Test PCIe Examples?

Part Number: 66AK2H12

Tool/software: TI-RTOS

Hi, All.

Here is my environment:

- Board : K2EVM-HK (SoC : 66AK2H12X)

- PDK : 4.0.4

- CCS : 7.1.0.00016

I would like to run the pcie example such as PCIE_K2H_wSoCFile_armExampleProject and PCIE_K2H_wSoCFile_C66BiosExampleProject.

Could you explain the best and fastest way to confirm the pcie example in EVMK2H environment?

<Execution Log>

[C66xx_0] **********************************************
* PCIe Test Start *
* EP mode *
**********************************************

Version #: 0x0202000c; string PCIE LLD Revision: 02.02.00.12:Mar 23 2018:21:19:58

Power domain is already enabled. You probably re-ran without device reset (which is OK)
PCIe Power Up.
Debug: Serdes Setup Successfully
PLL configured.
Successfully configured Inbound Translation!
Successfully configured Outbound Translation!
Starting link training...

............. And there are no logs.

Regards,

Donghwi