Part Number: PROCESSOR-SDK-AM65X
Tool/software: Linux
Hi Champs:
#1. We have tested the AM6 Linux SDK 5.2 version.
#2. While testing with the PRU Eth1 + Eth2, we found there are about 30% fail rate while doing the Giga Network testing in 5 mins.
#3. The testing env is:
PC (ubuntu) <------Cat 6 Ethernet Cable -------> AM6 + Linux SDK 5.2 PRU Eth1 or Eth2.
#4. And the Eth1 / Eth2 Throughput is about 80% performance compare to the Native Ethernet port on the AM6 EVM.
#5. Moreover, Customer is using the "CoreMark" tool to verify the AM6 Performance, do you have report while testing AM6 with CoreMark?
BR Rio