This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Should I expect DM365 H.264 video to work with Quicktime ?

I can see the H.264 output on VLC but am having trouble with Quicktime, on Windows or Mac. Seems to recognize only the audio portion. MPEG4 works.

Before diving too deep into this, I was wondering if someone already knows what the issue is and wether this is a permanent restriction or if compatibility is planned at some point.

Thanks

  • I don't see why it would'nt work with Quicktime off hand, it is just standard h.264 not even using the advanced options, though I have never actually tried it myself, in general I have only tested them with VLC. What sort of container format are you using, and how are you generating it, or are you just feeding in a raw .h264 file?

  • Hi

    We be  able to stream live video H.264  and audio  G.711 to Quicktime

    Make sure that sps/pps/idr frame are generated, follow this thread:  http://community.ti.com/forums/t/6453.aspx?PageIndex=1