This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Booting procedure for EVM Infotainment Kit J6EVM5777

Other Parts Discussed in Thread: J6EVM5777, X5777AXGABC

Hi,

I have a new J6EVM5777 Infotainment evaluation Kit, can you please share the procedure how to bring up this platform for android infotainment.

I have downloaded the prebuild image from software-dl.ti.com/infotainment/jacinto6/android/6AO_1_0_Release/binaries/6AO_1_0_emmc.tgz.

I want to know the procedure how to boot from memory card ( Android O).

Best Regards,

Shareen Taj A

  • Hi Shareen,

    please follow this document:
    processors.wiki.ti.com/.../6AO.1.0_Release_Notes

    Also note that there is 6AO.1.1 release:
    software-dl.ti.com/.../index_FDS.html

    Regards,
    Yordan
  • Shareen,

    To add :
    Current Android version is not designed for SD (Memory Card ) .
    Ref: e2e.ti.com/.../2504620

    Please use eMMC as pointed in the release notes above.
  • Hi Yordan,

    I have tried to boot the J6EVM5777 in the mentioned proceudre.

    I am getting the below logs, it seems android is not started, can you please help me to start the android services.

    I am booting the board after did the eMMC flash.

    Can you please guide me to get the android services.

    �
    U-Boot SPL 2016.05-00016-g6f6aaab (Nov 29 2017 - 20:39:40)
    DRA752-GP ES1.1
    no pinctrl for ddr_1_8v
    Trying to boot from SPI
    
    
    U-Boot 2016.05-00016-g6f6aaab (Nov 29 2017 - 20:39:40 -0600)
    
    CPU  : DRA752-GP ES1.1
    Model: TI DRA742
    Board: DRA74x EVM REV G.0
    DRAM:  1.5 GiB
    MMC:   mmc@4809c000: fail to find hs-rev11 mode FDT_ERR_NOTFOUND
    mmc@4809c000: fail to find sdr25-rev11 mode FDT_ERR_NOTFOUND
    mmc@4809c000: fail to find sdr12-rev11 mode FDT_ERR_NOTFOUND
    mmc@480b4000: fail to find hs-rev11 mode FDT_ERR_NOTFOUND
    OMAP SD/MMC: 0, OMAP SD/MMC: 1
    SCSI:  SATA link 0 timeout.
    AHCI 0001.0300 32 slots 1 ports 3 Gbps 0x1 impl SATA mode
    flags: 64bit ncq stag pm led clo only pmp pio slum part ccc apst 
    scanning bus for devices...
    Found 0 device(s).
    Net:   eth0: ethernet@48484000
    Hit any key to stop autoboot:  2  1  0 
    MMC: no card present
    MMC: no card present
    MMC: no card present
    switch to partitions #0, OK
    mmc1(part 0) is current device
    
    MMC read: dev # 1, block # 5376, count 512 ... 512 blocks read: OK
    
    MMC read: dev # 1, block # 101152, count 20480 ... 20480 blocks read: OK
    Booting from eMMC ...
    ## Booting Android Image at 0x82000000 ...
    Kernel load addr 0x80008000 size 7522 KiB
    Kernel command line: buildvariant=userdebug
    RAM disk load addr 0x83000000 size 1774 KiB
    ## Flattened Device Tree blob at 88000000
       Booting using the fdt blob at 0x88000000
       Loading Kernel Image ... OK
       Loading Ramdisk to 8fe44000, end 8ffff436 ... OK
       Loading Device Tree to 8fe26000, end 8fe43eb7 ... OK
    Using machid 0xfe6 from environment
    
    Starting kernel ...
    
    [    0.000000] Booting Linux on physical CPU 0x0
    [    0.000000] Initializing cgroup subsys cpuset
    [    0.000000] Initializing cgroup subsys cpu
    [    0.000000] Initializing cgroup subsys cpuacct
    [    0.000000] Linux version 4.4.91 (a0271468@magpie) (gcc version 4.9.x-google 20140827 (prerelease) (GCC) ) #1 SMP PREEMPT Wed Nov 29 20:36:56 CST 2017
    [    0.000000] CPU: ARMv7 Processor [412fc0f2] revision 2 (ARMv7), cr=30c5387d
    [    0.000000] CPU: PIPT / VIPT nonaliasing data cache, PIPT instruction cache
    [    0.000000] Machine model: TI DRA742
    [    0.000000] Reserved memory: created CMA memory pool at 0x0000000095800000, size 56 MiB
    [    0.000000] Reserved memory: initialized node ipu2_cma@95800000, compatible id shared-dma-pool
    [    0.000000] Reserved memory: created CMA memory pool at 0x0000000099000000, size 64 MiB
    [    0.000000] Reserved memory: initialized node dsp1_cma@99000000, compatible id shared-dma-pool
    [    0.000000] Reserved memory: created CMA memory pool at 0x000000009d000000, size 32 MiB
    [    0.000000] Reserved memory: initialized node ipu1_cma@9d000000, compatible id shared-dma-pool
    [    0.000000] Reserved memory: created CMA memory pool at 0x000000009f000000, size 8 MiB
    [    0.000000] Reserved memory: initialized node dsp2_cma@9f000000, compatible id shared-dma-pool
    [    0.000000] cma: Reserved 24 MiB at 0x00000000de400000
    [    0.000000] Forcing write-allocate cache policy for SMP
    [    0.000000] Memory policy: Data cache writealloc
    [    0.000000] OMAP4: Map 0x00000000dfd00000 to fe600000 for dram barrier
    [    0.000000] DRA752 ES1.1
    [    0.000000] PERCPU: Embedded 12 pages/cpu @ef1ab000 s20160 r8192 d20800 u49152
    [    0.000000] Built 1 zonelists in Zone order, mobility grouping on.  Total pages: 389440
    [    0.000000] Kernel command line: root=/dev/mmcblk0p2 rw init=/init rootfstype=ext4 rootwait drm.rnodes=1 androidboot.selinux=permissive snd.slots_reserved=1,1 snd-soc-core.pmdown_time=-1 uio_pdrv_genirq.of_id=generic-uio console=ttyS0,115200 androidboot.console=ttyS0 androidboot.hardware=jacinto6evmboard androidboot.serialno=0601401356dc0121 buildvariant=userdebug
    [    0.000000] PID hash table entries: 4096 (order: 2, 16384 bytes)
    [    0.000000] Dentry cache hash table entries: 131072 (order: 7, 524288 bytes)
    [    0.000000] Inode-cache hash table entries: 65536 (order: 6, 262144 bytes)
    [    0.000000] Memory: 1341256K/1564672K available (10240K kernel code, 620K rwdata, 3100K rodata, 2048K init, 668K bss, 35000K reserved, 188416K cma-reserved, 757760K highmem)
    [    0.000000] Virtual kernel memory layout:
    [    0.000000]     vector  : 0xffff0000 - 0xffff1000   (   4 kB)
    [    0.000000]     fixmap  : 0xffc00000 - 0xfff00000   (3072 kB)
    [    0.000000]     vmalloc : 0xf0800000 - 0xff800000   ( 240 MB)
    [    0.000000]     lowmem  : 0xc0000000 - 0xf0000000   ( 768 MB)
    [    0.000000]     pkmap   : 0xbfe00000 - 0xc0000000   (   2 MB)
    [    0.000000]     modules : 0xbf000000 - 0xbfe00000   (  14 MB)
    [    0.000000]       .text : 0xc0008000 - 0xc0c00000   (12256 kB)
    [    0.000000]       .init : 0xc1000000 - 0xc1200000   (2048 kB)
    [    0.000000]       .data : 0xc1200000 - 0xc129b3d4   ( 621 kB)
    [    0.000000]        .bss : 0xc129b3d4 - 0xc13425e8   ( 669 kB)
    [    0.000000] SLUB: HWalign=64, Order=0-3, MinObjects=0, CPUs=2, Nodes=1
    [    0.000000] Preemptible hierarchical RCU implementation.
    [    0.000000] 	Build-time adjustment of leaf fanout to 32.
    [    0.000000] NR_IRQS:16 nr_irqs:16 16
    [    0.000000] ti_dt_clocks_register: failed to lookup clock node gmac_gmii_ref_clk_div
    [    0.000000] OMAP clockevent source: timer1 at 32786 Hz
    [    0.000000] Architected cp15 timer(s) running at 6.14MHz (phys).
    [    0.000000] clocksource: arch_sys_counter: mask: 0xffffffffffffff max_cycles: 0x16af5adb9, max_idle_ns: 440795202250 ns
    [    0.000005] sched_clock: 56 bits at 6MHz, resolution 162ns, wraps every 4398046511023ns
    [    0.000016] Switching to timer-based delay loop, resolution 162ns
    [    0.000333] clocksource: 32k_counter: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 58327039986419 ns
    [    0.000342] OMAP clocksource: 32k_counter at 32768 Hz
    [    0.000780] Calibrating delay loop (skipped), value calculated using timer frequency.. 12.29 BogoMIPS (lpj=61475)
    [    0.000794] pid_max: default: 32768 minimum: 301
    [    0.000871] Security Framework initialized
    [    0.000882] SELinux:  Initializing.
    [    0.000961] Mount-cache hash table entries: 2048 (order: 1, 8192 bytes)
    [    0.000970] Mountpoint-cache hash table entries: 2048 (order: 1, 8192 bytes)
    [    0.001536] Initializing cgroup subsys io
    [    0.001554] Initializing cgroup subsys memory
    [    0.001580] Initializing cgroup subsys devices
    [    0.001593] Initializing cgroup subsys freezer
    [    0.001605] Initializing cgroup subsys perf_event
    [    0.001617] Initializing cgroup subsys pids
    [    0.001655] CPU: Testing write buffer coherency: ok
    [    0.001897] /cpus/cpu@0 missing clock-frequency property
    [    0.001914] /cpus/cpu@1 missing clock-frequency property
    [    0.001923] CPU0: update cpu_capacity 1024
    [    0.001932] CPU0: thread -1, cpu 0, socket 0, mpidr 80000000
    [    0.001978] Setting up static identity map for 0x80200000 - 0x80200060
    [    0.080067] CPU1: update cpu_capacity 1024
    [    0.080072] CPU1: thread -1, cpu 1, socket 0, mpidr 80000001
    [    0.080145] Brought up 2 CPUs
    [    0.080162] SMP: Total of 2 processors activated (24.59 BogoMIPS).
    [    0.080169] CPU: All CPU(s) started in HYP mode.
    [    0.080175] CPU: Virtualization extensions available.
    [    0.080208] CPU1: update max cpu_capacity 1024
    [    0.090077] CPU1: update max cpu_capacity 1024
    [    0.111320] VFP support v0.3: implementor 41 architecture 4 part 30 variant f rev 0
    [    0.112294] omap_hwmod: l3_main_2 using broken dt data from ocp
    [    0.318868] clocksource: jiffies: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 19112604462750000 ns
    [    0.318893] futex hash table entries: 512 (order: 3, 32768 bytes)
    [    0.322521] pinctrl core: initialized pinctrl subsystem
    [    0.323500] NET: Registered protocol family 16
    [    0.324675] DMA: preallocated 256 KiB pool for atomic coherent allocations
    [    0.350292] cpuidle: using governor ladder
    [    0.380321] cpuidle: using governor menu
    [    0.389403] OMAP GPIO hardware version 0.1
    [    0.393728] GPIO line 161 (radio_rst) hogged as output/low
    [    0.396155] irq: no irq domain found for /ocp/l4@4a000000/scm@2000/pinmux@1400 !
    [    0.413805] omap-gpmc 50000000.gpmc: GPMC revision 6.0
    [    0.413818] gpmc_mem_init: disabling cs 0 mapped at 0x0-0x1000000
    [    0.426273] hw-breakpoint: found 5 (+1 reserved) breakpoint and 4 watchpoint registers.
    [    0.426284] hw-breakpoint: maximum watchpoint size is 8 bytes.
    [    0.426777] omap4_sram_init:Unable to allocate sram needed to handle errata I688
    [    0.426787] omap4_sram_init:Unable to get sram pool needed to handle errata I688
    [    0.427454] OMAP DMA hardware revision 0.0
    [    0.472201] omap-dma-engine 4a056000.dma-controller: OMAP DMA engine driver (LinkedList1/2/3 supported)
    [    0.473436] edma 43300000.edma: memcpy is disabled
    [    0.478357] edma 43300000.edma: TI EDMA DMA engine driver
    [    0.483018] omap-iommu 40d01000.mmu: 40d01000.mmu registered
    [    0.483204] omap-iommu 40d02000.mmu: 40d02000.mmu registered
    [    0.483372] omap-iommu 58882000.mmu: 58882000.mmu registered
    [    0.483547] omap-iommu 55082000.mmu: 55082000.mmu registered
    [    0.483854] omap-iommu 41501000.mmu: 41501000.mmu registered
    [    0.484047] omap-iommu 41502000.mmu: 41502000.mmu registered
    [    0.486242] usbcore: registered new interface driver usbfs
    [    0.486303] usbcore: registered new interface driver hub
    [    0.486396] usbcore: registered new device driver usb
    [    0.487795] palmas 0-0058: IRQ missing: skipping irq request
    [    0.500846] palmas 0-0058: Muxing GPIO 2e, PWM 0, LED 0
    [    0.573243] pcf857x 0-0020: probed
    [    0.573818] pcf857x 0-0021: probed
    [    0.574173] omap_i2c 48070000.i2c: bus 0 rev0.12 at 400 kHz
    [    0.590870] GPIO line 463 (vin6_sel_s0) hogged as output/low
    [    0.590967] pcf857x 1-0026: probed
    [    0.591508] omap_i2c 48072000.i2c: bus 1 rev0.12 at 400 kHz
    [    0.591897] omap_i2c 48060000.i2c: bus 2 rev0.12 at 400 kHz
    [    0.610737] pcf857x: probe of 3-0021 failed with error -121
    [    0.610774] omap_i2c 4807a000.i2c: bus 3 rev0.12 at 400 kHz
    [    0.611003] media: Linux media interface: v0.10
    [    0.611061] Linux video capture interface: v2.00
    [    0.611102] pps_core: LinuxPPS API ver. 1 registered
    [    0.611110] pps_core: Software ver. 5.3.6 - Copyright 2005-2007 Rodolfo Giometti <giometti@linux.it>
    [    0.611139] PTP clock support registered
    [    0.611191] EDAC MC: Ver: 3.0.0
    [    0.621237] omap-mailbox 48840000.mailbox: omap mailbox rev 0x400
    [    0.621530] omap-mailbox 48842000.mailbox: omap mailbox rev 0x400
    [    0.621990] Advanced Linux Sound Architecture Driver Initialized.
    [    0.623427] clocksource: Switched to clocksource arch_sys_counter
    [    0.664486] NET: Registered protocol family 2
    [    0.665091] TCP established hash table entries: 8192 (order: 3, 32768 bytes)
    [    0.665156] TCP bind hash table entries: 8192 (order: 4, 65536 bytes)
    [    0.665281] TCP: Hash tables configured (established 8192 bind 8192)
    [    0.665329] UDP hash table entries: 512 (order: 2, 16384 bytes)
    [    0.665361] UDP-Lite hash table entries: 512 (order: 2, 16384 bytes)
    [    0.665513] NET: Registered protocol family 1
    [    0.666083] Trying to unpack rootfs image as initramfs...
    [    0.738337] Freeing initrd memory: 1776K
    [    0.739260] hw perfevents: enabled with armv7_cortex_a15 PMU driver, 7 counters available
    [    0.741993] audit: initializing netlink subsys (disabled)
    [    0.742048] audit: type=2000 audit(0.729:1): initialized
    [    0.749539] VFS: Disk quotas dquot_6.6.0
    [    0.749701] VFS: Dquot-cache hash table entries: 1024 (order 0, 4096 bytes)
    [    0.750779] squashfs: version 4.0 (2009/01/31) Phillip Lougher
    [    0.751036] ntfs: driver 2.1.32 [Flags: R/O].
    [    0.751373] fuse init (API version 7.23)
    [    0.755673] bounce: pool size: 64 pages
    [    0.755839] Block layer SCSI generic (bsg) driver version 0.4 loaded (major 247)
    [    0.755857] io scheduler noop registered
    [    0.755871] io scheduler deadline registered
    [    0.755907] io scheduler cfq registered (default)
    [    0.761094] pinctrl-single 4a003400.pinmux: 282 pins at pa fc003400 size 1128
    [    0.764611] PCI host bridge /ocp/axi@0/pcie_rc@51000000 ranges:
    [    0.764625]   No bus range found for /ocp/axi@0/pcie_rc@51000000, using [bus 00-ff]
    [    0.764658]    IO 0x20003000..0x20012fff -> 0x00000000
    [    0.764680]   MEM 0x20013000..0x2fffffff -> 0x20013000
    [    0.796857] dra7-pcie 51000000.pcie_rc: link is not up
    [    0.797029] dra7-pcie 51000000.pcie_rc: PCI host bridge to bus 0000:00
    [    0.797044] pci_bus 0000:00: root bus resource [bus 00-ff]
    [    0.797055] pci_bus 0000:00: root bus resource [io  0x0000-0xffff]
    [    0.797066] pci_bus 0000:00: root bus resource [mem 0x20013000-0x2fffffff]
    [    0.797470] PCI: bus0: Fast back to back transfers disabled
    [    0.797592] PCI: bus1: Fast back to back transfers enabled
    [    0.797679] pci 0000:00:00.0: BAR 0: assigned [mem 0x20100000-0x201fffff]
    [    0.797695] pci 0000:00:00.0: BAR 1: assigned [mem 0x20020000-0x2002ffff]
    [    0.797708] pci 0000:00:00.0: PCI bridge to [bus 01]
    [    0.797933] pcieport 0000:00:00.0: Signaling PME through PCIe PME interrupt
    [    0.802776] Serial: 8250/16550 driver, 10 ports, IRQ sharing disabled
    [    0.805308] console [ttyS0] disabled
    [    0.805359] 4806a000.serial: ttyS0 at MMIO 0x4806a000 (irq = 301, base_baud = 3000000) is a 8250
    [    1.832339] console [ttyS0] enabled
    [    1.836359] 4806c000.serial: ttyS1 at MMIO 0x4806c000 (irq = 302, base_baud = 3000000) is a 8250
    [    1.845687] 48020000.serial: ttyS2 at MMIO 0x48020000 (irq = 303, base_baud = 3000000) is a 8250
    [    1.855747] [drm] Initialized drm 1.1.0 20060810
    [    1.862487] OMAP DSS rev 6.1
    [    1.866292] omapdss_dss 58000000.dss: bound 58001000.dispc (ops dispc_component_ops)
    [    1.874767] omapdss_dss 58000000.dss: bound 58040000.encoder (ops hdmi5_component_ops)
    [    1.983911] brd: module loaded
    [    2.052057] loop: module loaded
    [    2.056740] nand: No NAND device found
    [    2.060513] omap2-nand 8000000.nand: scan failed, may be bus-width mismatch
    [    2.070587] m25p80 spi32766.0: s25fl256s1 (32768 Kbytes)
    [    2.076010] 7 ofpart partitions found on MTD device spi32766.0
    [    2.081870] Creating 7 MTD partitions on "spi32766.0":
    [    2.087051] 0x000000000000-0x000000040000 : "QSPI.SPL"
    [    2.093106] 0x000000040000-0x000000140000 : "QSPI.u-boot"
    [    2.099362] 0x000000140000-0x0000001c0000 : "QSPI.u-boot-spl-os"
    [    2.106209] 0x0000001c0000-0x0000001d0000 : "QSPI.u-boot-env"
    [    2.112771] 0x0000001d0000-0x0000001e0000 : "QSPI.u-boot-env.backup1"
    [    2.120072] 0x0000001e0000-0x0000009e0000 : "QSPI.kernel"
    [    2.126317] 0x0000009e0000-0x000002000000 : "QSPI.file-system"
    [    2.134034] libphy: Fixed MDIO Bus: probed
    [    2.138727] tun: Universal TUN/TAP device driver, 1.6
    [    2.143820] tun: (C) 1999-2004 Max Krasnyansky <maxk@qualcomm.com>
    [    2.150112] CAN device driver interface
    [    2.155067] c_can_platform 4ae3c000.can: c_can_platform device registered (regs=fce3c000, irq=365)
    [    2.213464] davinci_mdio 48485000.mdio: davinci mdio revision 1.6
    [    2.219589] davinci_mdio 48485000.mdio: detected phy mask fffffff3
    [    2.240143] libphy: 48485000.mdio: probed
    [    2.244222] davinci_mdio 48485000.mdio: phy[2]: device 48485000.mdio:02, driver unknown
    [    2.252263] davinci_mdio 48485000.mdio: phy[3]: device 48485000.mdio:03, driver unknown
    [    2.260992] cpsw 48484000.ethernet: Detected MACID = b4:99:4c:b5:59:b4
    [    2.267696] cpsw 48484000.ethernet: cpts: overflow check period 800
    [    2.274680] cpsw 48484000.ethernet: cpsw: Detected MACID = b4:99:4c:b5:59:b5
    [    2.282310] PPP generic driver version 2.4.2
    [    2.286758] PPP BSD Compression module registered
    [    2.291489] PPP Deflate Compression module registered
    [    2.296592] PPP MPPE Compression module registered
    [    2.301409] NET: Registered protocol family 24
    [    2.308253] ehci_hcd: USB 2.0 'Enhanced' Host Controller (EHCI) Driver
    [    2.314836] ehci-pci: EHCI PCI platform driver
    [    2.319346] ehci-platform: EHCI generic platform driver
    [    2.324942] ohci_hcd: USB 1.1 'Open' Host Controller (OHCI) Driver
    [    2.331171] ohci-pci: OHCI PCI platform driver
    [    2.336166] ohci-platform: OHCI generic platform driver
    [    2.342385] mousedev: PS/2 mouse device common for all mice
    [    2.348155] usbcore: registered new interface driver xpad
    [    2.353643] usbcore: registered new interface driver usb_acecad
    [    2.359629] usbcore: registered new interface driver aiptek
    [    2.365286] usbcore: registered new interface driver gtco
    [    2.370752] usbcore: registered new interface driver hanwang
    [    2.376501] usbcore: registered new interface driver kbtab
    [    2.382609] i2c /dev entries driver
    [    2.387191] vpe 489d0000.vpe: loading firmware vpdma-1b8.bin
    [    2.394280] vip 48970000.vip: loading firmware vpdma-1b8.bin
    [    2.400474] gspca_main: v2.14.0 registered
    [    2.404741] vpe 489d0000.vpe: Device registered as /dev/video0
    [    2.414068] device-mapper: uevent: version 1.0.3
    [    2.418940] device-mapper: ioctl: 4.34.0-ioctl (2015-10-28) initialised: dm-devel@redhat.com
    [    2.427459] vip 48970000.vip: VPDMA firmware loaded
    [    2.433852] omap_hsmmc 4809c000.mmc: Got CD GPIO
    [    2.439486] omap_hsmmc 480b4000.mmc: no pinctrl state for sdr25 mode
    [    2.445925] omap_hsmmc 480b4000.mmc: no pinctrl state for sdr12 mode
    [    2.452443] evm_3v3_sw: supplied by sysen1
    [    2.537213] mmc0: MAN_BKOPS_EN bit is not set
    [    2.547081] mmc0: new HS200 MMC card at address 0001
    [    2.552590] mmcblk0: mmc0:0001 MMC08G 7.25 GiB 
    [    2.557404] mmcblk0boot0: mmc0:0001 MMC08G partition 1 8.00 MiB
    [    2.563626] mmcblk0boot1: mmc0:0001 MMC08G partition 2 8.00 MiB
    [    2.573055]  mmcblk0: p1 p2 p3 p4 p5 p6 p7 p8 p9 p10 p11 p12 p13 p14 p15 p16 p17
    [    2.615362] ledtrig-cpu: registered to indicate activity on CPUs
    [    2.621485] hidraw: raw HID events driver (C) Jiri Kosina
    [    2.633381] usbcore: registered new interface driver usbhid
    [    2.640063] usbhid: USB HID core driver
    [    2.644208] ashmem: initialized
    [    2.652603] hwspinlock_user gatemp: requested 20 hwspinlocks
    [    2.658724] omap-rproc 58820000.ipu: assigned reserved memory node ipu1_cma@9d000000
    [    2.666566]  remoteproc0: 58820000.ipu is available
    [    2.671466]  remoteproc0: Note: remoteproc is still under development and considered experimental.
    [    2.680480]  remoteproc0: THE BINARY FORMAT IS NOT YET FINALIZED, and backward compatibility isn't yet guaranteed.
    [    2.691054]  remoteproc0: Direct firmware load for dra7-ipu1-fw.xem4 failed with error -2
    [    2.699324]  remoteproc0: Falling back to user helper
    [    2.699454] omap-rproc 55020000.ipu: assigned reserved memory node ipu2_cma@95800000
    [    2.699506]  remoteproc1: 55020000.ipu is available
    [    2.699510]  remoteproc1: Note: remoteproc is still under development and considered experimental.
    [    2.699513]  remoteproc1: THE BINARY FORMAT IS NOT YET FINALIZED, and backward compatibility isn't yet guaranteed.
    [    2.699658]  remoteproc1: Direct firmware load for dra7-ipu2-fw.xem4 failed with error -2
    [    2.699662]  remoteproc1: Falling back to user helper
    [    2.699927] omap-rproc 40800000.dsp: assigned reserved memory node dsp1_cma@99000000
    [    2.699975]  remoteproc2: 40800000.dsp is available
    [    2.699979]  remoteproc2: Note: remoteproc is still under development and considered experimental.
    [    2.699982]  remoteproc2: THE BINARY FORMAT IS NOT YET FINALIZED, and backward compatibility isn't yet guaranteed.
    [    2.700367] omap-rproc 41000000.dsp: assigned reserved memory node dsp2_cma@9f000000
    [    2.700420]  remoteproc3: 41000000.dsp is available
    [    2.700423]  remoteproc3: Note: remoteproc is still under development and considered experimental.
    [    2.700426]  remoteproc3: THE BINARY FORMAT IS NOT YET FINALIZED, and backward compatibility isn't yet guaranteed.
    [    2.714666]  remoteproc2: Direct firmware load for dra7-dsp1-fw.xe66 failed with error -2
    [    2.714670]  remoteproc2: Falling back to user helper
    [    2.714944]  remoteproc3: Direct firmware load for dra7-dsp2-fw.xe66 failed with error -2
    [    2.714947]  remoteproc3: Falling back to user helper
    [    2.768652] usbcore: registered new interface driver snd-usb-audio
    [    2.770427] davinci-mcasp 48464000.mcasp: DAI is shared
    [    2.771151] davinci-mcasp 48468000.mcasp: ERRATA i868 workaround is enabled
    [    2.771406] davinci-mcasp 48474000.mcasp: DAI is shared
    [    2.771432] davinci-mcasp 48474000.mcasp: ERRATA i868 workaround is enabled
    [    2.771633] davinci-mcasp 4847c000.mcasp: invalid tdm slots: 0
    [    2.782279] omap-hdmi-audio omap-hdmi-audio.0.auto: snd-soc-dummy-dai <-> 58040000.encoder mapping ok
    [    2.782988] u32 classifier
    [    2.782990]     input device check on
    [    2.782992]     Actions configured
    [    2.783009] Netfilter messages via NETLINK v0.30.
    [    2.783071] nf_conntrack version 0.5.0 (16384 buckets, 65536 max)
    [    2.783619] ctnetlink v0.93: registering with nfnetlink.
    [    2.784182] xt_time: kernel timezone is -0000
    [    2.917122] ip_tables: (C) 2000-2006 Netfilter Core Team
    [    2.922639] arp_tables: (C) 2002 David S. Miller
    [    2.927429] Initializing XFRM netlink socket
    [    2.932392] NET: Registered protocol family 10
    [    2.947933] mip6: Mobile IPv6
    [    2.950940] ip6_tables: (C) 2000-2006 Netfilter Core Team
    [    2.956802] sit: IPv6 over IPv4 tunneling driver
    [    2.962010] NET: Registered protocol family 17
    [    2.966519] NET: Registered protocol family 15
    [    2.970989] can: controller area network core (rev 20120528 abi 9)
    [    2.977264] NET: Registered protocol family 29
    [    2.981742] can: raw protocol (rev 20120528)
    [    2.986053] can: broadcast manager protocol (rev 20120528 t)
    [    2.991746] can: netlink gateway (rev 20130117) max_hops=1
    [    2.997565] NET: Registered protocol family 41
    [    3.002383] omap_voltage_late_init: Voltage driver support not added
    [    3.009381] Adding alias for supply vdd,cpu0 -> vdd,4a003b20.oppdm
    [    3.015622] Adding alias for supply vbb,cpu0 -> vbb,4a003b20.oppdm
    [    3.022376] Adding alias for supply vdd,cpu0 -> vdd,4a003b20.oppdm
    [    3.028640] Adding alias for supply vbb,cpu0 -> vbb,4a003b20.oppdm
    [    3.036216] Power Management for TI OMAP4+ devices.
    [    3.041371] Registering SWP/SWPB emulation handler
    [    3.046730] registered taskstats version 1
    [    3.051634] dmm 4e000000.dmm: workaround for errata i878 in use
    [    3.059509] dmm 4e000000.dmm: initialized all PAT entries
    [    3.267289] dwc3 48890000.usb: otg: primary host xhci-hcd.1.auto registered
    [    3.274307] dwc3 48890000.usb: otg: shared host xhci-hcd.1.auto registered
    [    3.281211] dwc3 48890000.usb: otg: can't start till gadget registers
    [    3.489371] xhci-hcd xhci-hcd.2.auto: xHCI Host Controller
    [    3.494911] xhci-hcd xhci-hcd.2.auto: new USB bus registered, assigned bus number 1
    [    3.502795] xhci-hcd xhci-hcd.2.auto: hcc params 0x0220f04c hci version 0x100 quirks 0x00210010
    [    3.511566] xhci-hcd xhci-hcd.2.auto: irq 511, io mem 0x488d0000
    [    3.517739] usb usb1: New USB device found, idVendor=1d6b, idProduct=0002
    [    3.524568] usb usb1: New USB device strings: Mfr=3, Product=2, SerialNumber=1
    [    3.531819] usb usb1: Product: xHCI Host Controller
    [    3.536955] usb usb1: Manufacturer: Linux 4.4.91 xhci-hcd
    [    3.542374] usb usb1: SerialNumber: xhci-hcd.2.auto
    [    3.547592] hub 1-0:1.0: USB hub found
    [    3.551383] hub 1-0:1.0: 1 port detected
    [    3.555576] xhci-hcd xhci-hcd.2.auto: xHCI Host Controller
    [    3.561091] xhci-hcd xhci-hcd.2.auto: new USB bus registered, assigned bus number 2
    [    3.568845] usb usb2: We don't know the algorithms for LPM for this host, disabling LPM.
    [    3.577075] usb usb2: New USB device found, idVendor=1d6b, idProduct=0003
    [    3.583904] usb usb2: New USB device strings: Mfr=3, Product=2, SerialNumber=1
    [    3.591155] usb usb2: Product: xHCI Host Controller
    [    3.596066] usb usb2: Manufacturer: Linux 4.4.91 xhci-hcd
    [    3.601486] usb usb2: SerialNumber: xhci-hcd.2.auto
    [    3.606688] hub 2-0:1.0: USB hub found
    [    3.610474] hub 2-0:1.0: 1 port detected
    [    3.615176] omap_hsmmc 4809c000.mmc: Got CD GPIO
    [    3.655137] input: gpio_keys as /devices/platform/gpio_keys/input/input0
    [    3.661995] hctosys: unable to open rtc device (rtc0)
    [    3.677886] evm_1v8: disabling
    [    3.680958] aic_dvdd: disabling
    [    3.684130] vmmcwl_fixed: disabling
    [    3.687653] evm_3v3_sd: disabling
    [    3.691122] ALSA device list:
    [    3.694119]   #1: HDMI 58040000.encoder
    [    3.699318] Freeing unused kernel memory: 2048K
    [    3.706117] init: init first stage started!
    [    3.792430] init: Coldboot took 0.0786347 seconds
    [    3.803732] EXT4-fs (mmcblk0p10): mounted filesystem with ordered data mode. Opts: (null)
    [    3.811985] init: [libfs_mgr]__mount(source=/dev/block/platform/44000000.ocp/480b4000.mmc/by-name/system,target=/system,type=ext4)=0
    [    3.830278] EXT4-fs (mmcblk0p11): mounted filesystem with ordered data mode. Opts: (null)
    [    3.838543] init: [libfs_mgr]__mount(source=/dev/block/platform/44000000.ocp/480b4000.mmc/by-name/vendor,target=/vendor,type=ext4)=0
    [    3.850586] init: Skipped setting INIT_AVB_VERSION (not in recovery mode)
    [    3.857432] init: Loading SELinux policy
    [    3.949724] audit: type=1403 audit(3.939:2): policy loaded auid=4294967295 ses=4294967295
    [    3.958181] selinux: SELinux: Loaded policy from /sepolicy
    [    3.958181] 
    [    3.967536] selinux: SELinux: Loaded file_contexts
    [    3.967536] 
    [    3.974945] random: init: uninitialized urandom read (40 bytes read, 9 bits of entropy available)
    [    3.985057] init: init second stage started!
    [    3.995987] selinux: SELinux: Loaded file_contexts
    [    3.995987] 
    [    4.002694] selinux: SELinux: Loaded property_contexts from /plat_property_contexts & /nonplat_property_contexts.
    [    4.002694] 
    [    4.014528] init: Running restorecon...
    [    4.046333] init: waitpid failed: No child processes
    [    4.051981] init: Couldn't load properties from /odm/default.prop: No such file or directory
    [    4.061886] init: Created socket '/dev/socket/property_service', mode 666, user 0, group 0
    [    4.070360] init: Parsing file /init.rc...
    [    4.074848] init: Added '/init.environ.rc' to import list
    [    4.080287] init: Added '/init.usb.rc' to import list
    [    4.085394] init: Added '/init.jacinto6evmboard.rc' to import list
    [    4.091613] init: Added '/vendor/etc/init/hw/init.jacinto6evmboard.rc' to import list
    [    4.099506] init: Added '/init.usb.configfs.rc' to import list
    [    4.105393] init: Added '/init.zygote32.rc' to import list
    [    4.112094] init: Parsing file /init.environ.rc...
    [    4.117032] init: Parsing file /init.usb.rc...
    [    4.121898] init: Parsing file /init.jacinto6evmboard.rc...
    [    4.127539] init: could not import file '/init.jacinto6evmboard.rc' from '/init.rc': No such file or directory
    [    4.138682] init: Parsing file /vendor/etc/init/hw/init.jacinto6evmboard.rc...
    [    4.146418] init: Added '/vendor/etc/init/hw/init.jacinto6evmboard.usb.rc' to import list
    [    4.154935] init: Parsing file /vendor/etc/init/hw/init.jacinto6evmboard.usb.rc...
    [    4.163164] init: Parsing file /init.usb.configfs.rc...
    [    4.169042] init: Parsing file /init.zygote32.rc...
    [    4.174098] init: Parsing directory /system/etc/init...
    [    4.179831] init: Parsing file /system/etc/init/android.hidl.allocator@1.0-service.rc...
    [    4.188413] init: Parsing file /system/etc/init/atrace.rc...
    [    4.195513] init: Parsing file /system/etc/init/atrace_userdebug.rc...
    [    4.202657] init: Parsing file /system/etc/init/audioserver.rc...
    [    4.209303] init: Parsing file /system/etc/init/bootanim.rc...
    [    4.215639] init: Parsing file /system/etc/init/bootstat.rc...
    [    4.221991] init: Parsing file /system/etc/init/cameraserver.rc...
    [    4.228678] init: Parsing file /system/etc/init/drmserver.rc...
    [    4.235126] init: Parsing file /system/etc/init/dumpstate.rc...
    [    4.241535] init: Parsing file /system/etc/init/gatekeeperd.rc...
    [    4.248101] init: Parsing file /system/etc/init/hwservicemanager.rc...
    [    4.255133] init: Parsing file /system/etc/init/init-debug.rc...
    [    4.261606] init: Parsing file /system/etc/init/installd.rc...
    [    4.268257] init: Parsing file /system/etc/init/keystore.rc...
    [    4.274584] init: Parsing file /system/etc/init/lmkd.rc...
    [    4.280531] init: Parsing file /system/etc/init/logcatd.rc...
    [    4.286918] init: Parsing file /system/etc/init/logd.rc...
    [    4.292957] init: Parsing file /system/etc/init/logtagd.rc...
    [    4.299206] init: Parsing file /system/etc/init/mdnsd.rc...
    [    4.305271] init: Parsing file /system/etc/init/mediadrmserver.rc...
    [    4.312112] init: Parsing file /system/etc/init/mediaextractor.rc...
    [    4.318968] init: Parsing file /system/etc/init/mediametrics.rc...
    [    4.325641] init: Parsing file /system/etc/init/mediaserver.rc...
    [    4.332229] init: Parsing file /system/etc/init/mtpd.rc...
    [    4.338217] init: Parsing file /system/etc/init/netd.rc...
    [    4.344200] init: Parsing file /system/etc/init/perfprofd.rc...
    [    4.350581] init: Parsing file /system/etc/init/racoon.rc...
    [    4.356747] init: Parsing file /system/etc/init/servicemanager.rc...
    [    4.363598] init: Parsing file /system/etc/init/storaged.rc...
    [    4.369895] init: Parsing file /system/etc/init/surfaceflinger.rc...
    [    4.376797] init: Parsing file /system/etc/init/tombstoned.rc...
    [    4.383288] init: Parsing file /system/etc/init/uncrypt.rc...
    [    4.389575] init: Parsing file /system/etc/init/vdc.rc...
    [    4.395474] init: Parsing file /system/etc/init/vold.rc...
    [    4.401447] init: Parsing file /system/etc/init/webview_zygote32.rc...
    [    4.408490] init: Parsing file /system/etc/init/wifi-events.rc...
    [    4.415954] init: Parsing file /system/etc/init/wificond.rc...
    [    4.422315] init: Parsing directory /vendor/etc/init...
    [    4.427638] init: Parsing file /vendor/etc/init/android.hardware.audio@2.0-service.rc...
    [    4.436275] init: Parsing file /vendor/etc/init/android.hardware.automotive.evs@1.0-service.rc...
    [    4.445641] init: Parsing file /vendor/etc/init/android.hardware.automotive.vehicle@2.0-service.rc...
    [    4.455365] init: Parsing file /vendor/etc/init/android.hardware.camera.provider@2.4-service.rc...
    [    4.464820] init: Parsing file /vendor/etc/init/android.hardware.configstore@1.0-service.rc...
    [    4.473914] init: Parsing file /vendor/etc/init/android.hardware.graphics.allocator@2.0-service.rc...
    [    4.483648] init: Parsing file /vendor/etc/init/android.hardware.keymaster@3.0-service.rc...
    [    4.492545] init: Parsing file /vendor/etc/init/android.hardware.media.omx@1.0-service.rc...
    [    4.501477] init: Parsing file /vendor/etc/init/android.hardware.usb@1.0-service.rc...
    [    4.509867] init: Parsing file /vendor/etc/init/android.hardware.wifi@1.0-service.rc...
    [    4.518355] init: Parsing file /vendor/etc/init/hostapd.android.rc...
    [    4.525284] init: Parsing file /vendor/etc/init/vndservicemanager.rc...
    [    4.532380] init: Parsing file /odm/etc/init...
    [    4.537020] init: processing action (early-init)
    [    4.542060] init: starting service 'ueventd'...
    [    4.547212] init: failed to open /acct/uid_0/pid_130/cgroup.procs: No such file or directory
    [    4.548225] random: ueventd: uninitialized urandom read (40 bytes read, 12 bits of entropy available)
    [    4.549832] ueventd: ueventd started!
    [    4.550356] ueventd: /sys/ rule /sys/devices/platform/trusty.* trusty_version
    [    4.550375] ueventd: /sys/ rule /sys/devices/virtual/input/input* enable
    [    4.550392] ueventd: /sys/ rule /sys/devices/virtual/input/input* poll_delay
    [    4.550409] ueventd: /sys/ rule /sys/devices/virtual/usb_composite/* enable
    [    4.550434] ueventd: /sys/ rule /sys/devices/system/cpu/cpu* cpufreq/scaling_max_freq
    [    4.550450] ueventd: /sys/ rule /sys/devices/system/cpu/cpu* cpufreq/scaling_min_freq
    [    4.557998] selinux: SELinux: Loaded file_contexts
    [    4.557998] 
    [    4.562690] selinux: SELinux: Loaded file_contexts
    [    4.562690] 
    [    4.565255] ueventd: fixup /sys/devices/system/cpu/cpu0/cpufreq/scaling_max_freq 1000 1000 664
    [    4.565401] ueventd: fixup /sys/devices/system/cpu/cpu0/cpufreq/scaling_min_freq 1000 1000 664
    [    4.565809] ueventd: fixup /sys/devices/system/cpu/cpu1/cpufreq/scaling_max_freq 1000 1000 664
    [    4.565897] ueventd: fixup /sys/devices/system/cpu/cpu1/cpufreq/scaling_min_freq 1000 1000 664
    [    4.659681] init: createProcessGroup(0, 130) failed for service 'ueventd': No such file or directory
    [    4.668948] init: Command 'start ueventd' action=early-init (/init.rc:30) returned 0 took 126.902ms.
    [    4.678296] init: processing action (wait_for_coldboot_done)
    [    4.725931] ueventd: firmware: loading 'dra7-dsp2-fw.xe66' for '/devices/platform/44000000.ocp/41000000.dsp/remoteproc3/firmware/dra7-dsp2-fw.xe66'
    [    4.747419] ueventd: firmware: loading 'dra7-ipu2-fw.xem4' for '/devices/platform/44000000.ocp/55020000.ipu/remoteproc1/firmware/dra7-ipu2-fw.xem4'
    [    4.781416] ueventd: firmware: loading 'dra7-dsp1-fw.xe66' for '/devices/platform/44000000.ocp/40800000.dsp/remoteproc2/firmware/dra7-dsp1-fw.xe66'
    [    4.796808] ueventd: firmware: loading 'dra7-ipu1-fw.xem4' for '/devices/platform/44000000.ocp/58820000.ipu/remoteproc0/firmware/dra7-ipu1-fw.xem4'
    [    4.820799] ueventd: Coldboot took 0.26264 seconds
    [    4.830145] init: Command 'wait_for_coldboot_done' action=wait_for_coldboot_done returned 0 took 146.107ms.
    [    4.840272] init: processing action (mix_hwrng_into_linux_rng)
    [    4.846209] init: /dev/hw_random not found
    [    4.850363] init: processing action (set_mmap_rnd_bits)
    [    4.855914] init: processing action (set_kptr_restrict)
    [    4.861427] init: processing action (keychord_init)
    [    4.866427] init: processing action (console_init)
    [    4.871295] init: processing action (init)
    [    4.881051] init: write_file: Unable to open '/proc/sys/kernel/hung_task_timeout_secs': No such file or directory
    [    4.897555] init: write_file: Unable to open '/proc/sys/abi/swp': No such file or directory
    [    4.906128] init: write_file: Unable to open '/sys/class/leds/vibrator/trigger': No such file or directory
    [    4.916899] init: processing action (mix_hwrng_into_linux_rng)
    [    4.922850] init: /dev/hw_random not found
    [    4.927471] init: processing action (late-init)
    [    4.932329] ueventd: loading /devices/platform/44000000.ocp/55020000.ipu/remoteproc1/firmware/dra7-ipu2-fw.xem4 took 0.185136 seconds
    [    4.932842] init: starting service 'exec 1 (/vendor/bin/modprobe)'...
    [    4.933668] init: SVC_EXEC pid 136 (uid 0 gid 0+0 context u:r:vendor_modprobe:s0) started; waiting...
    [    4.951392] random: modprobe: uninitialized urandom read (40 bytes read, 13 bits of entropy available)
    [    4.971053]  remoteproc1: powering up 55020000.ipu
    [    4.975895]  remoteproc1: Booting fw image dra7-ipu2-fw.xem4, size 3730752
    [    4.982868] omap-iommu 55082000.mmu: 55082000.mmu: version 2.1
    [    4.986734] SCSI subsystem initialized
    [    4.991247] usbcore: registered new interface driver usb-storage
    [    5.009671] GPIO line 461 (LVDS_CLKSel) hogged as output/high
    [    5.021415] backlight supply power not found, using dummy regulator
    [    5.028608] leds backlight: Failed setting brightness
    [    5.043014] input: LDC 3001 TouchScreen Controller as /devices/platform/44000000.ocp/48070000.i2c/i2c-0/0-0018/input/input1
    [    5.046078]  remoteproc1: remote processor 55020000.ipu is now up
    [    5.062331] ov1063x 1-0037: Failed writing register 0x0103!
    [    5.062366] virtio_rpmsg_bus virtio0: rpmsg host is online
    [    5.062380]  remoteproc1: registered virtio0 (type 7)
    [    5.065494] [drm] Supports vblank timestamp caching Rev 2 (21.10.2013).
    [    5.065496] [drm] No driver support for vblank timestamp query.
    [    5.078712] [drm] Enabling DMM ywrap scrolling
    [    5.095732] virtio_rpmsg_bus virtio0: creating channel rpmsg-rpc addr 0x65
    [    5.095867] rpmsg_rpc rpmsg0: probing service dce-callback with src 1024 dst 101
    [    5.095979] virtio_rpmsg_bus virtio0: creating channel rpmsg-rpc addr 0x66
    [    5.096086] rpmsg_rpc rpmsg1: probing service rpmsg-dce with src 1025 dst 102
    [    5.096215] ov1063x: probe of 1-0037 failed with error -121
    [    5.096401] rpmsg_rpc rpmsg0: published functions = 4
    [    5.096559] rpmsg_rpc rpmsg1: published functions = 9
    [    5.098801] tvp5158 1-0058: Unable to of_probe
    [    5.103181] aic_dvdd: supplied by evm_3v3_sw
    [    5.105064] init: Service 'exec 1 (/vendor/bin/modprobe)' (pid 136) exited with status 1 waiting took 0.172799 seconds
    [    5.105116] init: processing action (queue_property_triggers)
    [    5.105163] init: processing action (fs)
    [    5.139231] init: [libfs_mgr]superblock s_max_mnt_count:10,/dev/block/platform/44000000.ocp/480b4000.mmc/by-name/cache
    [    5.139248] init: [libfs_mgr]do_quota_with_shutdown_check(): was not clealy shutdown, state flag:1incompat flag:46
    [    5.139259] init: [libfs_mgr]Requested quota status is match on /dev/block/platform/44000000.ocp/480b4000.mmc/by-name/cache
    [    5.144521] EXT4-fs (mmcblk0p12): Ignoring removed nomblk_io_submit option
    [    5.213866] omapdrm omapdrm.0: fb0: omapdrm frame buffer device
    [    5.268668] [drm] Initialized omapdrm 1.0.0 20110917 on minor 0
    [    5.276126] asoc-simple-card sound0: tlv320aic3x-hifi <-> 48468000.mcasp mapping ok
    [    5.292133] asoc-simple-card jamr3_sound: tlv320aic3x-hifi <-> 48474000.mcasp mapping ok
    [    5.303635] tvp5158 1-0058: Unable to of_probe
    [    5.577069] EXT4-fs (mmcblk0p12): recovery complete
    [    5.582867] EXT4-fs (mmcblk0p12): mounted filesystem with ordered data mode. Opts: errors=remount-ro,nomblk_io_submit
    [    5.593684] init: [libfs_mgr]check_fs(): mount(/dev/block/platform/44000000.ocp/480b4000.mmc/by-name/cache,/cache,ext4)=0: Success
    [    5.634919] init: [libfs_mgr]check_fs(): unmount(/cache) succeeded
    [    5.641220] init: [libfs_mgr]Running /system/bin/e2fsck on /dev/block/platform/44000000.ocp/480b4000.mmc/by-name/cache
    [    5.672700] random: e2fsck: uninitialized urandom read (40 bytes read, 18 bits of entropy available)
    [    5.747076] random: e2fsck: uninitialized urandom read (40 bytes read, 20 bits of entropy available)
    [    5.802283] e2fsck: e2fsck 1.43.3 (04-Sep-2016)
    [    5.802283] 
    [    5.808378] e2fsck: Pass 1: Checking inodes, blocks, and sizes
    [    5.808378] 
    [    5.815885] e2fsck: Pass 2: Checking directory structure
    [    5.815885] 
    [    5.822713] e2fsck: Pass 3: Checking directory connectivity
    [    5.822713] 
    [    5.829874] e2fsck: Pass 4: Checking reference counts
    [    5.829874] 
    [    5.836480] e2fsck: Pass 5: Checking group summary information
    [    5.836480] 
    [    5.843944] e2fsck: cache: 14/16384 files (0.0% non-contiguous), 2093/65536 blocks
    [    5.843944] 
    [    5.856048] EXT4-fs (mmcblk0p12): mounted filesystem with ordered data mode. Opts: (null)
    [    5.864362] init: [libfs_mgr]__mount(source=/dev/block/platform/44000000.ocp/480b4000.mmc/by-name/cache,target=/cache,type=ext4)=0
    [    5.877301] init: [libfs_mgr]superblock s_max_mnt_count:10,/dev/block/platform/44000000.ocp/480b4000.mmc/by-name/userdata
    [    5.888341] init: [libfs_mgr]do_quota_with_shutdown_check(): was not clealy shutdown, state flag:1incompat flag:46
    [    5.898755] init: [libfs_mgr]Requested quota status is match on /dev/block/platform/44000000.ocp/480b4000.mmc/by-name/userdata
    [    5.910635] EXT4-fs (mmcblk0p17): Ignoring removed nomblk_io_submit option
    [    6.188969] EXT4-fs (mmcblk0p17): recovery complete
    [    6.194805] EXT4-fs (mmcblk0p17): mounted filesystem with ordered data mode. Opts: errors=remount-ro,nomblk_io_submit
    [    6.205608] init: [libfs_mgr]check_fs(): mount(/dev/block/platform/44000000.ocp/480b4000.mmc/by-name/userdata,/data,ext4)=0: Success
    [    6.247947] init: [libfs_mgr]check_fs(): unmount(/data) succeeded
    [    6.254148] init: [libfs_mgr]Running /system/bin/e2fsck on /dev/block/platform/44000000.ocp/480b4000.mmc/by-name/userdata
    [    6.267166] random: e2fsck: uninitialized urandom read (40 bytes read, 34 bits of entropy available)
    [    6.288488] random: e2fsck: uninitialized urandom read (40 bytes read, 34 bits of entropy available)
    [    6.649351] e2fsck: e2fsck 1.43.3 (04-Sep-2016)
    [    6.649351] 
    [    6.655424] e2fsck: Pass 1: Checking inodes, blocks, and sizes
    [    6.655424] 
    [    6.662767] e2fsck: Pass 2: Checking directory structure
    [    6.662767] 
    [    6.669600] e2fsck: Pass 3: Checking directory connectivity
    [    6.669600] 
    [    6.676711] e2fsck: Pass 4: Checking reference counts
    [    6.676711] 
    [    6.683357] e2fsck: Pass 5: Checking group summary information
    [    6.683357] 
    [    6.690715] e2fsck: /dev/block/platform/44000000.ocp/480b4000.mmc/by-name/userdata: 1351/387840 files (2.8% non-contiguous), 67058/1549463 blocks
    [    6.690715] 
    [    6.708360] EXT4-fs (mmcblk0p17): mounted filesystem with ordered data mode. Opts: (null)
    [    6.716681] init: [libfs_mgr]__mount(source=/dev/block/platform/44000000.ocp/480b4000.mmc/by-name/userdata,target=/data,type=ext4)=0
    [    6.729255] init: Parsing file /odm/etc/init...
    [    6.733931] init: Command 'mount_all /vendor/etc/fstab.jacinto6evmboard' action=fs (/vendor/etc/init/hw/init.jacinto6evmboard.rc:31) returned 0 took 1628.71ms.
    [    6.748717] init: processing action (post-fs)
    [    6.754013] init: Couldn't load properties from /odm/build.prop: No such file or directory
    [    6.763117] init: Couldn't load properties from /factory/factory.prop: No such file or directory
    [    6.773925] init: computing context for service 'logd'
    [    6.780117] init: starting service 'logd'...
    [    6.785294] init: computing context for service 'servicemanager'
    [    6.785782] init: Created socket '/dev/socket/logd', mode 666, user 1036, group 1036
    [    6.786150] init: Created socket '/dev/socket/logdr', mode 666, user 1036, group 1036
    [    6.786518] init: Created socket '/dev/socket/logdw', mode 222, user 1036, group 1036
    [    6.786628] init: Opened file '/proc/kmsg', flags 0
    [    6.786668] init: Opened file '/dev/kmsg', flags 1
    [    6.824859] init: starting service 'servicemanager'...
    [    6.830900] init: computing context for service 'hwservicemanager'
    [    6.833802] random: logd: uninitialized urandom read (40 bytes read, 55 bits of entropy available)
    [    6.837463] random: servicemanager: uninitialized urandom read (40 bytes read, 55 bits of entropy available)
    [    6.856307] init: starting service 'hwservicemanager'...
    [    6.860115] random: logd: uninitialized urandom read (40 bytes read, 56 bits of entropy available)
    [    6.871508] init: computing context for service 'vndservicemanager'
    [    6.878063] init: starting service 'vndservicemanager'...
    [    6.890287] logd.auditd: start
    [    6.904150] logd.klogd: 6900724275
    [    6.935625] init: Command 'restorecon --recursive --cross-filesystems /sys/kernel/debug' action=post-fs (/init.rc:315) returned 0 took 51.1608ms.
    [    6.951172] selinux: SELinux: Skipping restorecon_recursive(/cache)
    [    6.951172] 
    [    6.967608] init: write_file: Unable to open '/sys/kernel/tracing/tracing_on': No such file or directory
    [    6.978606] init: processing action (late-fs)
    [    6.978656] binder: 153:153 ioctl 620a 357297e7 returned -22
    [    6.989485] init: computing context for service 'keymaster-3-0'
    [    6.995625] init: starting service 'keymaster-3-0'...
    [    7.002183] init: processing action (post-fs-data)
    [    7.007409] init: computing context for service 'vold'
    [    7.012706] init: starting service 'vold'...
    [    7.020285] init: Created socket '/dev/socket/vold', mode 660, user 0, group 1009
    [    7.028576] init: Created socket '/dev/socket/cryptd', mode 660, user 0, group 1009
    [    7.148062] vdc: 200 164 Command succeeded
    [    7.152397] init: init_user0 result: 0
    [    7.156725] selinux: SELinux: Skipping restorecon_recursive(/data)
    [    7.156725] 
    [    7.164751] init: computing context for service 'exec 2 (/system/bin/tzdatacheck)'
    [    7.172535] init: starting service 'exec 2 (/system/bin/tzdatacheck)'...
    [    7.180254] init: SVC_EXEC pid 168 (uid 1000 gid 1000+0 context default) started; waiting...
    [    7.201924] init: Service 'exec 2 (/system/bin/tzdatacheck)' (pid 168) exited with status 0 waiting took 0.037242 seconds
    [    7.217790] init: processing action (ro.crypto.state=unsupported && zygote-start)
    [    7.225458] init: ExecStart(update_verifier_nonencrypted): Service not found
    [    7.232655] init: computing context for service 'netd'
    [    7.238128] init: starting service 'netd'...
    [    7.243294] init: computing context for service 'zygote'
    [    7.243823] init: Created socket '/dev/socket/netd', mode 660, user 0, group 1000
    [    7.244211] init: Created socket '/dev/socket/dnsproxyd', mode 660, user 0, group 3003
    [    7.244542] init: Created socket '/dev/socket/mdns', mode 660, user 0, group 1000
    [    7.244933] init: Created socket '/dev/socket/fwmarkd', mode 660, user 0, group 3003
    [    7.279718] init: starting service 'zygote'...
    [    7.285070] init: do_start: Service zygote_secondary not found
    [    7.285786] init: Created socket '/dev/socket/zygote', mode 660, user 0, group 1000
    [    7.302666] init: processing action (load_persist_props_action)
    [    7.309881] init: Couldn't load properties from /data/local.prop: No such file or directory
    [    7.443905] init: Command 'load_persist_props' action=load_persist_props_action (/init.rc:250) returned 0 took 134.015ms.
    [    7.456216] init: computing context for service 'logd-reinit'
    [    7.462882] init: starting service 'logd-reinit'...
    [    7.468778] init: processing action (firmware_mounts_complete)
    [    7.474881] init: processing action (early-boot)
    [    7.485384] init: processing action (boot)
    [    7.489512] ueventd: firmware: could not find firmware for dra7-dsp2-fw.xe66
    [    7.490193] init: write_file: Unable to open '/proc/sys/vm/min_free_order_shift': No such file or directory
    [    7.493537] init: computing context for service 'hidl_memory'
    [    7.493703] init: starting service 'hidl_memory'...
    [    7.494516] init: computing context for service 'audio-hal-2-0'
    [    7.494705] init: starting service 'audio-hal-2-0'...
    [    7.495439] init: computing context for service 'evs-hal-1-0'
    [    7.495606] init: service evs-hal-1-0 does not have a SELinux domain defined
    [    7.495676] init: computing context for service 'vehicle-hal-2.0'
    [    7.495812] init: starting service 'vehicle-hal-2.0'...
    [    7.496522] init: computing context for service 'camera-provider-2-4'
    [    7.496727] init: starting service 'camera-provider-2-4'...
    [    7.497444] init: computing context for service 'configstore-hal-1-0'
    [    7.497630] init: starting service 'configstore-hal-1-0'...
    [    7.498323] init: computing context for service 'gralloc-2-0'
    [    7.498521] init: starting service 'gralloc-2-0'...
    [    7.499209] init: computing context for service 'usb-hal-1-0'
    [    7.499406] init: starting service 'usb-hal-1-0'...
    [    7.500097] init: computing context for service 'wifi_hal_legacy'
    [    7.500305] init: starting service 'wifi_hal_legacy'...
    [    7.501131] init: computing context for service 'healthd'
    [    7.501308] init: starting service 'healthd'...
    [    7.502001] init: computing context for service 'pvrsrvinit'
    [    7.502191] init: starting service 'pvrsrvinit'...
    [    7.502920] init: computing context for service 'lmkd'
    [    7.503102] init: starting service 'lmkd'...
    [    7.504734] init: couldn't write 178 to /dev/cpuset/camera-daemon/tasks: No such file or directory
    [    7.517730] init: computing context for service 'surfaceflinger'
    [    7.517936] init: starting service 'surfaceflinger'...
    [    7.525282] init: computing context for service 'exec 3 (/vendor/bin/init.jacinto6evmboard.cpuset.sh)'
    [    7.525476] init: starting service 'exec 3 (/vendor/bin/init.jacinto6evmboard.cpuset.sh)'...
    [    7.528362] init: SVC_EXEC pid 187 (uid 0 gid 0+1 context default) started; waiting...
    [    7.529185] ueventd: firmware: could not find firmware for dra7-ipu1-fw.xem4
    [    7.529258] ueventd: loading /devices/platform/44000000.ocp/58820000.ipu/remoteproc0/firmware/dra7-ipu1-fw.xem4 took 2.73267 seconds
    [    7.529648]  remoteproc0: failed to load dra7-ipu1-fw.xem4
    [    7.529976] init: Failed to bind socket 'pdx/system/vr/display/client': No such file or directory
    [    7.530279] init: Failed to bind socket 'pdx/system/vr/display/manager': No such file or directory
    [    7.530563] init: Failed to bind socket 'pdx/system/vr/display/vsync': No such file or directory
    [    7.534230] init: Created socket '/dev/socket/lmkd', mode 660, user 1000, group 1000
    [    7.542139] logd.daemon: reinit
    [    7.545590] init: Service 'logd-reinit' (pid 173) exited with status 0
    [    7.546108] ueventd: firmware: could not find firmware for dra7-dsp1-fw.xe66
    [    7.546175] ueventd: loading /devices/platform/44000000.ocp/40800000.dsp/remoteproc2/firmware/dra7-dsp1-fw.xe66 took 2.76499 seconds
    [    7.773522]  remoteproc2: failed to load dra7-dsp1-fw.xe66
    [    7.812373]  remoteproc3: failed to load dra7-dsp2-fw.xe66
    [    7.818130] ueventd: loading /devices/platform/44000000.ocp/41000000.dsp/remoteproc3/firmware/dra7-dsp2-fw.xe66 took 3.09243 seconds
    [    7.859761] healthd: unable to get HAL interface, using defaults
    [    7.885835] tvp5158 1-0058: Unable to of_probe
    [    7.916050] healthd: No battery devices found
    [    7.919205] PVR_K: UM DDK-(4081762) and KM DDK-(4081762) match. [ OK ]
    [    7.927816] type=1400 audit(7.909:3): avc: denied { create } for pid=177 comm="android.hardwar" scontext=u:r:hal_vehicle_default:s0 tcontext=u:r:hal_vehicle_default:s0 tclass=tcp_socket permissive=1
    [    7.956320] healthd: battery l=100 v=0 t=42.4 h=2 st=2 chg=a
    [    7.976734] type=1400 audit(7.909:3): avc: denied { create } for pid=177 comm="android.hardwar" scontext=u:r:hal_vehicle_default:s0 tcontext=u:r:hal_vehicle_default:s0 tclass=tcp_socket permissive=1
    [    7.996167] init: Service 'exec 3 (/vendor/bin/init.jacinto6evmboard.cpuset.sh)' (pid 187) exited with status 0 waiting took 0.470962 seconds
    [    8.008398] type=1400 audit(7.909:4): avc: denied { bind } for pid=177 comm="android.hardwar" scontext=u:r:hal_vehicle_default:s0 tcontext=u:r:hal_vehicle_default:s0 tclass=tcp_socket permissive=1
    [    8.008503] type=1400 audit(7.909:4): avc: denied { bind } for pid=177 comm="android.hardwar" scontext=u:r:hal_vehicle_default:s0 tcontext=u:r:hal_vehicle_default:s0 tclass=tcp_socket permissive=1
    [    8.008510] type=1400 audit(7.909:5): avc: denied { node_bind } for pid=177 comm="android.hardwar" src=33452 scontext=u:r:hal_vehicle_default:s0 tcontext=u:object_r:node:s0 tclass=tcp_socket permissive=1
    [    8.008575] type=1400 audit(7.909:5): avc: denied { node_bind } for pid=177 comm="android.hardwar" src=33452 scontext=u:r:hal_vehicle_default:s0 tcontext=u:object_r:node:s0 tclass=tcp_socket permissive=1
    [    8.008581] type=1400 audit(7.909:6): avc: denied { listen } for pid=177 comm="android.hardwar" lport=33452 scontext=u:r:hal_vehicle_default:s0 tcontext=u:r:hal_vehicle_default:s0 tclass=tcp_socket permissive=1
    [    8.008652] type=1400 audit(7.909:6): avc: denied { listen } for pid=177 comm="android.hardwar" lport=33452 scontext=u:r:hal_vehicle_default:s0 tcontext=u:r:hal_vehicle_default:s0 tclass=tcp_socket permissive=1
    [    8.008658] type=1400 audit(7.909:7): avc: denied { accept } for pid=177 comm="android.hardwar" lport=33452 scontext=u:r:hal_vehicle_default:s0 tcontext=u:r:hal_vehicle_default:s0 tclass=tcp_socket permissive=1
    [    8.137675] init: Service 'pvrsrvinit' (pid 184) exited with status 0
    [    8.145329] init: insmod: open("/vendor/lib/modules/cmemk.ko") failed: No such file or directory
    [    8.154335] init: insmod: open("/system/lib/modules/galcore.ko") failed: No such file or directory
    [    8.165114] file system registered
    [    8.180276] init: processing action (persist.sys.usb.config=* && boot)
    [    8.187388] init: processing action (enable_property_trigger)
    [    8.195928] init: processing action (security.perf_harden=1)
    [    8.201899] init: processing action (ro.debuggable=1)
    [    8.208101] init: starting service 'console'...
    [    8.13969] init: processing action (sys.usb.config=adb && sys.usb.configfs=1)
    [    8.221375] init: starting service 'adbd'...
    [    8.226709] init: processing action (nonencrypted)
    [    8.231677] init: cannot find '/system/bin/install-recovery.sh', disabling 'flash_recovery': No such file or directory
    [    8.242650] init: computing context for service 'lad_dra7xx'
    [    8.243669] init: Created socket '/dev/socket/adbd', mode 660, user 1000, group 1000
    [    8.246855] read descriptors
    [    8.246864] read descriptors
    [    8.246869] read strings
    [    8.248534] init: setpgid failed for console: Operation not permitted
    [    8.271327] init: starting service 'lad_dra7xx'...
    [    8.277170] init: computing context for service 'audioserver'
    [    8.283208] init: starting service 'audioserver'...
    [    8.289145] init: computing context for service 'cameraserver'
    [    8.295532] init: starting service 'cameraserver'...
    [    8.301566] init: computing context for service 'drm'
    [    8.304294] init: couldn't write 240 to /dev/cpuset/camera-daemon/tasks: No such file or directory
    [    8.315963] init: starting service 'drm'...
    [    8.321108] init: computing context for service 'installd'
    [    8.327055] init: starting service 'installd'...
    [    8.332552] init: computing context for service 'keystore'
    [    8.338335] init: starting service 'keystore'...
    [    8.343965] init: computing context for service 'mediadrm'
    [    8.349740] init: starting service 'mediadrm'...
    [    8.355303] init: computing context for service 'mediaextractor'
    [    8.361590] init: starting service 'mediaextractor'...
    [    8.367727] init: computing context for service 'mediametrics'
    [    8.373904] init: starting service 'mediametrics'...
    [    8.379751] init: computing context for service 'media'
    [    8.385300] init: starting service 'media'...
    [    8.390489] init: computing context for service 'storaged'
    [    8.396277] init: starting service 'storaged'...
    [    8.401810] init: computing context for service 'wificond'
    [    8.407643] init: starting service 'wificond'...
    [    8.413233] init: computing context for service 'mediacodec'
    [    8.419742] init: starting service 'mediacodec'...
    [    8.425527] init: Command 'class_start main' action=nonencrypted (/init.rc:623) returned 0 took 193.803ms.
    [    8.436074] init: computing context for service 'gatekeeperd'
    [    8.442053] init: starting service 'gatekeeperd'...
    jacinto6evm:/ $ [    8.536613] init: cannot find '/system/xbin/perfprofd', disabling 'perfprofd': No such file or directory
    [    8.557010] init: computing context for service 'tombstoned'
    [    8.603899] init: starting service 'tombstoned'...
    [    8.609707] init: Command 'class_start late_start' action=nonencrypted (/init.rc:624) returned 0 took 173.651ms.
    [    8.653911] init: Opened file '/d/mmc0/mmc0:0001/ext_csd', flags 0
    [    8.706473] init: processing action (sys.usb.config=adb && sys.usb.configfs=1 && sys.usb.ffs.ready=1)
    [    8.805098] init: Created socket '/dev/socket/tombstoned_crash', mode 666, user 1000, group 1000
    [    8.888197] dwc3 48890000.usb: otg: gadget gadget registered
    [    8.954112] init: Created socket '/dev/socket/tombstoned_intercept', mode 666, user 1000, group 1000
    [    8.994477] init: Command 'write /config/usb_gadget/g1/UDC ${sys.usb.controller}' action=sys.usb.config=adb && sys.usb.configfs=1 && sys.usb.ffs.ready=1 (/init.usb.configfs.rc:20) returned 0 took 106.269ms.
    [    9.225455] init: computing context for service 'bootanim'
    [    9.231174] init: starting service 'bootanim'...
    [    9.284830] healthd: battery l=100 v=0 t=42.4 h=2 st=2 chg=a
    [    9.381344] android_work: sent uevent USB_STATE=CONNECTED
    [    9.391440] android_work: sent uevent USB_STATE=DISCONNECTED
    [    9.520620] android_work: sent uevent USB_STATE=CONNECTED
    [    9.531899] configfs-gadget gadget: high-speed config #1: b
    [    9.538486] android_work: sent uevent USB_STATE=CONFIGURED
    [   10.310250] random: nonblocking pool is initialized
    [   12.392630] capability: warning: `main' uses 32-bit capabilities (legacy support in use)
    [   17.799153] healthd: battery l=100 v=0 t=42.4 h=2 st=2 chg=a
    [   18.890588] init: processing action (sys.sysctl.extra_free_kbytes=*)
    [   20.098469] net eth1: initializing cpsw version 1.15 (0)
    [   20.104051] net eth0: initialized cpsw ale version 1.4
    [   20.109535] net eth0: ALE Table size 1024
    [   20.117388] tvp5158 1-0058: Unable to of_probe
    [   20.129002] net eth1: phy found : id is : 0x20005c7a
    [   20.141198] IPv6: ADDRCONF(NETDEV_UP): eth1: link is not ready
    [   20.168195] IPv6: ADDRCONF(NETDEV_UP): eth1: link is not ready
    [   20.352770] init: computing context for service 'webview_zygote32'
    [   20.375107] init: starting service 'webview_zygote32'...
    [   20.391024] init: Created socket '/dev/socket/webview_zygote', mode 660, user 1053, group 1000
    [   21.166609] omap-iommu 55082000.mmu: 55082000.mmu: version 2.1
    [   23.971999] init: Service 'bootanim' (pid 280) exited with status 0
    [   24.026867] init: processing action (sys.boot_completed=1)
    [   24.039352] init: processing action (sys.boot_completed=1 && sys.logbootcomplete=1)
    [   24.054465] init: computing context for service 'exec 4 (/system/bin/bootstat)'
    [   24.062276] init: starting service 'exec 4 (/system/bin/bootstat)'...
    [   24.073125] init: SVC_EXEC pid 738 (uid 0 gid 0+0 context default) started; waiting...
    [   24.106513] init: Service 'exec 4 (/system/bin/bootstat)' (pid 738) exited with status 0 waiting took 0.052279 seconds
    [   24.119080] init: computing context for service 'exec 5 (/system/bin/bootstat)'
    [   24.128933] init: starting service 'exec 5 (/system/bin/bootstat)'...
    [   24.139856] init: SVC_EXEC pid 741 (uid 0 gid 0+0 context default) started; waiting...
    [   24.191573] init: Service 'exec 5 (/system/bin/bootstat)' (pid 741) exited with status 0 waiting took 0.072470 seconds
    [   24.207493] init: computing context for service 'exec 6 (/system/bin/bootstat)'
    [   24.220614] init: starting service 'exec 6 (/system/bin/bootstat)'...
    [   24.228799] init: SVC_EXEC pid 742 (uid 0 gid 0+0 context default) started; waiting...
    [   24.282873] init: Command 'exec - root root -- /system/bin/bootstat --record_time_since_factory_reset' action=sys.boot_completed=1 && sys.logbootcomplete=1 (/system/etc/init/bootstat.rc:42) returned 0 took 75.9569ms.
    [   24.325872] init: Service 'exec 6 (/system/bin/bootstat)' (pid 742) exited with status 0 waiting took 0.118364 seconds
    [   24.339905] init: computing context for service 'exec 7 (/system/bin/bootstat)'
    [   24.348181] init: starting service 'exec 7 (/system/bin/bootstat)'...
    [   24.357087] init: SVC_EXEC pid 763 (uid 0 gid 0+0 context default) started; waiting...
    [   24.380740] init: Service 'exec 7 (/system/bin/bootstat)' (pid 763) exited with status 0 waiting took 0.040836 seconds
    [   24.393001] init: processing action (sys.boot_completed=1 && sys.wifitracing.started=0)
    [   24.462567] init: Command 'mkdir /sys/kernel/debug/tracing/instances/wifi 711' action=sys.boot_completed=1 && sys.wifitracing.started=0 (/system/etc/init/wifi-events.rc:22) returned 0 took 54.2802ms.
    [   26.422870] init: Command 'restorecon_recursive /sys/kernel/debug/tracing/instances/wifi' action=sys.boot_completed=1 && sys.wifitracing.started=0 (/system/etc/init/wifi-events.rc:23) returned 0 took 1941.71ms.
    

  • From the log, it appears that you are using "DRA74x EVM REV G.0".
    1. did you flash the right dtb in environment partition ? as shown at : processors.wiki.ti.com/.../6AO.1.0_Application_Notes " dra7-evm-lcd-lg.dtb "
    2. do you have the right cpu board + lcd panel configuration as pointed in release notes in supported platforms?
  • Hi,

    Please find my comments for your questions,


    1. did you flash the right dtb in environment partition? as shown at : processors.wiki.ti.com/.../6AO.1.0_Application_Notes " dra7-evm-lcd-lg.dtb "

    => I run the fasboot.sh file, and it flash correct dra7-evm-lcd-lg.dtb file in the MMC from the linux PC via USB 3.0.
    After that I couldn't find any problems in the log reg .dtb file is wrong.

    2. do you have the right cpu board + lcd panel configuration as pointed in release notes in supported platforms?
    => The processor is "X5777AXGABC" and I have connected the HDMI output from the target. We didn't connect the correct LCD Panel

    Question 1:
    Here my question is, to up the all required android services, do we need to connect the right lcd panel?
    Just want to check the log information whether android services is up and running without connecting the right LCD Panel.
    After booting If I run the ps command from the shell, I am getting the following log as it is shown only two process's running in the target

    jacinto6evm:/ $ ps
    USER PID PPID VSZ RSS WCHAN ADDR S NAME
    shell 246 1 4372 2264 sigsuspend ab4176f4 S sh
    shell 1233 246 5368 2648 0 ac9973c4 R ps

    Question 2:
    In order to get the HDMI output, do we need any special configuration in the target?

    Question 3:
    We don't have compatible lcd panel right now, so do we have any other option to get the display from the target apart from HDMI output? ( eg. via VNC server)
  • Hi,

    Thanks for your support, we had a problem with lcd display unit. We got the output successfully.

    Regards,
    Shareen