Other Parts Discussed in Thread: OMAP-L138
The C6748 or the DSP side of L-138 doesn’t seem to have whole lot of packages in CCS4.2. The one that I especially need is for the on-chip USB2.0 controller. Can you comment as to the availability of USB2 stack? Or some example codes for the USB2 port, to initialize, to enumerate, to handle various interrupts generated by the USB2 module? We intend to use the USB2 port as just a Device, not OTG, run under SYS/BIOS.
Thanks again!
Paul