Tool/software: Code Composer Studio
What boot-mode is used in EVMK2H? ARM-master or C66x-master?
If ARM-master mode is used and If I load the operating system Linux as is described in "Linux Getting Started Guide"
software-dl.ti.com/.../Overview_Getting_Started_Guide.html
then will the kernels c66x be involved in work?
Can I work with c66x under the control of the Linux system?
Second question.
In EVMK2H There is provided "0010:NOR SPI BOOT" mode (or No Boot/JTAG).
And if I load the operating system Linux as described in "Linux Getting Started Guide" is it loaded only in NOR whithout using NAND?
(NOR-flash is small !)
And one more.
Where BMC code of EVMK2H is located? In flash (NOR or NAND)?
If this code will be corrupted how can I restore it?
Regards, Alexander.