Other Parts Discussed in Thread: TMS320DM8168
As I understand it, the Integra DSP+ARM (TMS320C6A816x) Processors do not support IEEE 1588. Is that correct? If so, is there any way to add the necessary time stamping other than with a separate MAC?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: TMS320DM8168
As I understand it, the Integra DSP+ARM (TMS320C6A816x) Processors do not support IEEE 1588. Is that correct? If so, is there any way to add the necessary time stamping other than with a separate MAC?
You have listed several devices that do NOT support IEEE1588, so which devices DO support IEEE1588? And do we have software to support this as well?
~Leonard
LeonardEllis said:You have listed several devices that do NOT support IEEE1588
These several devices are the devices that this e2e forum support:
"This forum supports the pin-to-pin and software compatible DM816x, C6A816x and AM389x devices."
LeonardEllis said:so which devices DO support IEEE1588? And do we have software to support this as well?
I can find that IEEE1588 we have in DM814x/AM387x/DM38x, AM335x, AM437x, DRA7x. See the below pointers for more details:





Regards,
Pavel