This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Creating a ramdisk

I’d like to set up a ramdisk to use for a fast file storage/retrieval filesystem. I have this in my bootargs:

ramdisk_size=16000

During bootup I see this:

RAMDISK driver initialized: 1 RAM disks of 16000K size 1024 blocksize

At the moment there are no   /dev/ramx   devices showing up in the  /dev directory. Doing a bit of Googling it looks like I now have to create a file system, maybe something like this, but it gives me a “Could not stat” error:

# mkfs.ext2 /dev/ram0
mke2fs 1.35 (28-Feb-2004)
Could not stat /dev/ram0 --- No such file or directory. The device apparently does not exist; did you specify it correctly?
#

Could you advise me please on the configuration and steps to create a general purpose ramdisk on the EVM? Many thanks.