Part Number: TMS320C6678
1) It is said that some of the libraries for C66x based DSPs are open source and some do require commercial licences. Does anybody know how I can get information about which are the open source libraries and which require commercial licenses?
2) Is there anyway to use OPENCL on a device without ARM Cortex like TMS320C6678 which consists 8 C66x cores.
3) The lsat question is about how C66x is set as fixed or floating point. Is there an instruciton set that makes C66x core to change its state from fixed to floating point in the same code?
Thanks.