Part Number: BEAGLEBOARD-X15
Other Parts Discussed in Thread: AM5728,
Tool/software: Linux
Hi!
I've recently gotten a BeagleBoard X-15 with the AM5728 mounted on it for some application development in-house, within TI. I'm facing some fairly fundamental issues that are preventing me from proceeding. It would be great if you could point me to the right resources/let me know how I can resolve the same: I'm also not too familiar with Linux, so any material on that front is also welcome!
- Is there some kernel update of some sorts I need to do out of the box, or is the X15 ready to go as is? There's nothing mentioned at this link. If so, what are the steps to be followed?
- I am not ale to use PuTTY to connect to the X-15 as mentioned in the link above, either. This is not a concern for me since my application doesn't demand it, but I'm not sure if that's indicative of something else.
- How do I connect to the internal TI network? I tried adding proxies in the ~/.bashrc file and sourcing the same, but am not able to get the BeagleBoard through the firewall.
- As an extension of the above, I'm not able to edit the /etc/apt/apt.conf.d/70debconf file to configure apt-get for package download, as mentioned in this link. I do not know the root/user password for the device to su or sudo.
Please help me with the above. I understand that not all questions may be answered here, since this is an external forum - please feel free to mail me.
Thanks!
Madhu