This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRA75: Are external PullUp/Down resistors always needed for TMS(F18), TRST(D20) and TCLK(E20) pins?

Part Number: DRA75

Dear Sirs or Madams,

According to Table 4-1 shown on DRA75x datasheet revised NOVEMBER 2018, 

TMS(F18), TRST(D20) and TCLK(E20) pins require external PullUp/Down resistors "when unused".

Considering that these pins are related to JTAG function and they can be considered as "unused" when JTAG device is NOT connected to DRA75 externally,

we now understand that  external PullUp/Down resistors have to be connected to these pins regardless whether JTAG function of DRA75 is used or NOT.

Is our above understanding cprrect? 

Best regards,

Shinsuke Tanaka