This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Configuring TVP5146 with DM355 for NTSC on S-Video



I have a DMM355_EVM that works fine with PAL composite input. The MPEG4 Encoder sample runs just fine. When I disconnect the PAL camera and connect an NTSC camera to the S-Video port, the encoder sample starts up, my driver detects that there is now an NTSC camera connected to the S-Video port but I never get any frames out. I get the same result when I connect an NTSC signal to the composite port so I'm guessing that I've missed some configuration step but have yet to find the appropriate point in the documentation that tells me what I need to do. I'm using the Windows Embedded CE 6.0 BSP.

Any suggestions/pointers would be greatly appreciated.

Regards,

Mike Markley