Part Number: AM5718
Hi Sitara Support Team,
This post is related question of the thread.
e2e.ti.com/.../2634861
My customer would like to know that possibility o realize plane combining
like the requirements below by using the hardware built in AM 5718
and reducing the CPU load?
I understand that the maximum planes are 2 planes on one display
and the customer requirement can be accept the following status.
Can the DSS and 2D/3D accelerator of AM5718 manage the following requirements?
If it can, can my customer request the detail information
for the Vivante Corp. GC320; 2D accelerator to TI?
I have just refer this thread.
e2e.ti.com/.../473705
****Customer's requirement****
AM571x can realize the all planes output.
-Resolution: First LVDS(or CMOS) output(1366x768),
Second CMOS output(1020x1080)
-Framerate: 60Hz
-Color Space Format: 15bit Color RGB
-At least four types of pallets can be specified for each layer.
-The palettes can have alpha data.
-It can Change the display position by changing display reference coordinates
for "menu2".
-When "0h" is specified for pixel data, the data of the lower plane is displayed.
<Planes Specs>
Plane0 for mouse (cursor)
Plane1 for "Menu1"
Plane2 for "Menu2"
Plane3 for waveform
Plane4 for waveform
Plane5 for Numeric value
Plane6 for Frame
<First LVDS(or CMOS) output(1366x768)
- Conbined 6 planes and mouse cursor =>LVDS(or CMOS) output(1366x768)
<Second CMOS output(1020x1080)
- Conbined 5 planes except for Plane1 and mouse
=======> Scaling; 1920x1080 =====>LVDS(or CMOS) output(1366x768)
||
====================>Hard copy; Dump to Memory(Output file such as JPG, PNG)
***********************************************
Best regards,
Kanae