This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TDA3XEVM: Can Graphics Source Link create custom graphics ?

Part Number: TDA3XEVM

Following is comment on top of grpxSrcLink.h:

Grpx source Link can be used for the following  purposes
 *     1. For testing a link that does not take capture data
 *     2. For generating logo and sending it to Display
 *     3. For printing stats on the display

My question:  Grpx Source Link can be used for the following purposes?

1.  To turn ON pixels at specific position on display

2.  To create and display shapes such as circle, rectangles, etc.

3.  To create and display text

Does TI SDK have support for fonts?  If these fonts don't suit my needs, can I add my own fonts to TI SDK?

 

Regards,

Amer