This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Installing Target Linux Software, DVSDK Software in AMD 64 X2



I want to install the necessary software to work with my card DVEVM DM355, indicated in the manual spruf73c.pdf.
This software I want installed on my PC with Linux OS and the AMD Athlon (tm) 64 X2 Dual Core Processor 5600 +.
Following the instructions in the manual section 4.3, is that I can not install the software, the software that came with my card is for 32-bit Intel processors. They could tell me where can I get the appropriate software for my host?.

mvl_5_0_0801921_demo_sys_setuplinux.bin
mvl_5_0_0_demo_lsp_setuplinux_02_00_00_140.bin
dvsdk_setuplinux_2_00_00_22.bin
xdctools_setuplinux_3_10_05_61.bin
data.tar.gz
LPTB-02.03.00.02-beta.bin
dm355_flash_image_2_00_00_22.tar

and others.

Thanks,

Ramac