Other Parts Discussed in Thread: OMAP-L137, OMAP-L138
I've read a number of articles, got the idea that you need to use AISgen to make a boot file..
But I don't see where there's a utility - or utility framework - for loading the AISgen created image to the SPI flash device... I have found discussions about using a serial port loader that takes the image, and loads it to the SPI device, but I can't find anything that actually does that.. Unfortunately after spinning my wheels quite a bit, that's all I can seem to get.,,.
To complicate matters (or not), I am trying to load a simple application on to an OMAP-L137 without using DSP BIOS, or Linux, just load a simple control loop app on to the DSP core, boot, and run like hell. I have found CSL (deprecated) CSL support, and I have an app under CCS v4 that I can build run / debug over the JTAG on to an eval board.
So.. where do I find a SPI flash loader app for my soon to be created AISgen image?
Anyone? :) .. Thanks in advance..