Other Parts Discussed in Thread: SN74AUP1G97
Hello,
I'm trying to understand if the following setup will work and what is involved at driver level to support it. Basically I'd like to connect DM365's AEMIF to DM6435's HPI and preserve NAND functionality on DM365. My idea is to use current CE0 to select the NAND chip (no change from EVM setup) and connect CE1 to DM6435's SPI along with required signals. But since the AEMIF controller is the same, I am not sure if "normal mode" and "NAND flash mode" can be used at the same time or in mutual exclusion or what involves switching from one mode to the other.
I've checked DM365's AEMIF document but I am not sure of what will this setup impact at driver level. I'd like to preserve current MTD functionality and add communication through AEMIF/HPI on the other chip select.
Any help, comment or suggestion will be appreciated.