This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM5748: AM5748 PCIe clock question and related IBIS file question

Part Number: AM5748

Dear Champs,

We're using PCIe on our custom AM5748 board. I have two questions in regards to the PCIe clock, specifically pins

AH15 LJCB_CLKN

AG15 LJCB_CLKP

1. The TRM says we can drive the PCIe clock as an output. When I checked with our various EVMs, we always have the PCIe configured as an input. My question is, are we okay using PCIe as an output? Is it proven?

2. The AM5748 IBIS file (am574x.ibs) only has models for the PCIe clock pins configured as inputs. I'd like to ask why there aren't models for these pins configured as outputs?

AG15     LJCB_CLKP           ACSPCIE_RX_M#753   0.558230000000000000 0.000000003040000000 0.000000000001286000

AH15     LJCB_CLKN           ACSPCIE_RX_M#753   0.576810000000000000 0.000000003218000000 0.000000000001301000