Part Number: TMS320C6678
Hi,
Referring to table 2 in the document below:
Can you clarify if I need to divide the Mcycles by the clock frequency of 1250MHz to get the average frame decode latency? Or do we need to take into account the number of cores used in each configuration?
Configuration _006 is the closest to our use case and according to the table it takes ~600ms to decode a frame.
Why do the low delay cases have higher average Mcycle counts?
Video is 480 by 480, 30Hz, mono coming in over Ethernet. We decode the video, add overlays, and then display over an analog channel. No encoding is required at this time.
Thanks,
Jeramie