Part Number: TMS320C6748
I have a DSP board with C6748 on it. The boot configuration pins are all 1s (Boot[7:0] = 11111111) on the board. Two questions:
1) The firmware is stored on a NOR flash which is attached to SPI1 of C6748.
In Appendix A of SPRAAT2F, we have boot mode selection table where we see Boot[7:0] = 00001100 as the SPI1 flsah boot mode.
The DSP loads from NOR flash even though C6748 boot configuration pins Boot[7:0] = 11111111 not 00001100 on our board.
How come this happens.
2) Again on the same board, I can use XDs5120USB Jtag debugger, with boot configuration as Boot[7:0] = 11111111 . Emulation debug boot confiuration mode is given as Boot[7:0]=00011110.
Does boot configuration mode must definitely be equal to Boot[7:0]=00011110 (Emulation Debug) to use the Jtag debugger with the DSP.
It looks like no since I can use Jtag on our board.
Best regards
Izzet