Part Number: AM3517
Hi Experts,
Could you please let me know about the VIH(min) for USB0_VBUS?
Does AM3517 work if USB0_VBUS is 3.3V?
According to the datasheet in 5.1 Absolute Maximum Ratings, USB VBUS pin (usb0_vbus) (max) is 5.5V.
I believe that the port could detect the line even though it is 3.3V because of the 5V tolerant function.
Hope it works.
Best regards,
Hitoshi