This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Linux/TMDSIDK574: Difference of ECC function between AM574x and AM6x

Part Number: TMDSIDK574

Tool/software: Linux

Hi TI Experts, 

I am looking for the solution with high memory reliability to replace the current one, AM437x. Currently, both AM574x and AM6x can support full DDR ecc. What is the difference between of them?

Thanks

  • Hi Kang,

    DDR ECC feature between these two devices (AM574x and AM57x) is similar, but there are some differences. You can compare the TRMs sections:

    AM574x
    15.1.3 EMIF Overview
    15.3.4.14 Error Correction And Detection Feature


    AM65x
    8.2.1 DDRSS Overview
    8.2.4.1.5 Data Error Detection and Correction

    Regards,
    Pavel