Part Number: TDA3
Other Parts Discussed in Thread: AWR1243
Hi,
We are trying to reduce the overall framePrediodicity (frame rate) of a chirp configuration. From looking at the below equation which I found from one of the existing support thread.
(rampEndTime*10 + idleTimeConst*10)*(chirpEndIdx-chirpStartIdx+1)*loopCount < framePeriodicty, I would like to keep the rest of the parameters the same other than the loopCounter. we tried to reduce the loopCount which is currently set to 128 in our usecase. This loopCounter actually correspond to number of chirps in a frame. We would like to use 16 chirps to reduce to frame time by a factor of 8. However, the current vision sdk does NOT currently support such a small number of FFT samples.
How hard is it to add support for 16 and 32 sample FFT?
Thanks,
--Khai