Hi,
I was successful in executing an early boot with emac basic example integrated with ipc example loaded through sd card where in I had previously encountered an issue of resource table which was solved here and the executable is read successfully.
But the issue now is I am not able to see the output which was previously shown by the .out file without ipc.
On adding the IPC to EMAC example what could have prevented it from showing the blinking output on connecting the ethernet.
I am using processor sdk rtos automotive-dra7xx-evm-04.03.00.05
Regards,
Padmesh