This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM3352: DDR3L tCK

Guru 16770 points
Part Number: AM3352

Hi

According to following wiki, tCK=400MHz is selected instead of 800MHz for DDR3-1600.

http://processors.wiki.ti.com/index.php/Sitara_Linux_Training:_Tuning_the_DDR3_Timings_on_BeagleBoneBlack#Updating_SPL.2FU-boot

Actually, MT41K256M16HA-125 would operate in 800MHz.

Could it mean that tCK should be limited up to 400MHz as maximum with AM3352?

BestRegards