Part Number: 66AK2E05
Hi,
Could you clarify what is causing a delay? We measure 476ms delay from reset release to the first SPI read, where the ROM bootloader is trying to load just a 35KB image. I don’t see how that could be boot size dependent because the ROM code won’t know what size to pull until it reads from Flash.
RESETSTAT goes active a handful of ms after reset release, so the part is coming out of reset as expected. BOOTCOMPLETE was instrumented as well but discovered that it only goes active after all of the cores are booted.
Thanks,
Jeramie