This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

RTOS/AM5728: am5728

Part Number: AM5728

Tool/software: TI-RTOS

Hi,

Please explain me that what the macro function HW_SYNC_BARRIER  is all about ? present in the hw_types.h file.

Thanks,

Ranganath

  • Hi Ranganath,

    HW_SYNC_BARRIER is executing DSB (Data Synchronization Barrier) assembly instruction. The DSB instruction is a special memory barrier, that synchronizes the execution stream with memory  accesses.

    pdk_am57xx_1_0_13/packages/ti/csl/hw_types.h

    /**
     *  \brief This macro to use data sync barrier in case of ARM.
     *         This can not be defined as static inline function. This will be
     *         called inside every hardware register writes.
     *         In case cache APIs are implemented to use the hardware register
     *         write functions, (current implementation) and we call a function
     *         after actual reg write for cache disable,
     *         the return address in the stack will be invalid.
     */
    #if (defined(__ARMv7) || defined(__TI_ARM_V7__))
    #ifndef MEM_BARRIER_DISABLE
    #define HW_SYNC_BARRIER()                                                      \
    {                                                                              \
        asm("    dsb");                                                            \
    }

     

    See also below e2e threads for more info:

    And we have also info in ARM docs:

    Regards,
    Pavel

  • thanks Pavel Botev.

    I am using  PROCESSOR-SDK-RTOS-AM57X - pdk_am57xx_1_0_7.

    Here, I have slave device over SPI3_CS0. Data rate configured as 32 bits, Phase and Polarity are 0 and bit rate is 1Mhz.

    Now, when I try to run loopback SPI3 test, data corruption is observed for SPI3, same code if I try with SPI2 its working properly. based on my debug when HW_WR_REG32_RAW() called it will write Tx data to address 0x480B138 and when In Rx path , it will called HW_RD_REG32_RAW() reading data from 0x480B13C for SPI3. but sometimes after HW_SYNC_BARRIER(); in HW_WR_REG32_RAW() API data corruption happen. Can you please see loopback code for SPI3 which I am attaching. MCSPI_BasicLoopbackExample_am5728.zip 

     

  • Ranganath,

    I see you have already open e2e thread regarding this McSPI issue:

    e2e.ti.com/.../2817250

    Please continue with your original thread and close this one.

    Regards,
    Pavel