This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM3352: ODTLon

Guru 16770 points

Part Number: AM3352

Hi

Regarding to TRM (SPRUH73P), REG:SDRAM_TIM_2, BIT:27-25 is reserved with 2h, so we never access it.

And these bits represents ODTLon in DDR3 timing configuration tool.

So I think we need to set "2" to ODTLon cell in configuration tool in any case.

Is my understanding correct?

BestRegards