Part Number: DRA74
Tool/software: Linux
Hi,experts,
I download psdk0500 from ti.com. and install completed!,
When I boot from sd, I found the uboot version still is 201605, and the kernel is still 4.4.84,
I checked the release notes, as below
SDK Components & Versions
| Component | Version |
|---|---|
| Linux Kernel | 4.14.79+ (2018 LTS) |
| U-Boot | 2018.01+ |
| Yocto Project | 2.4 (Rocko) |
| Linaro Toolchain (gcc) | 7.2.1 hard-float |
| Qt | 5.9.7 |
| Wayland | 2.0 |
| GStreamer | 1.12 |
Could you help to check the issue?
Widic